<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Use segger J-link instead of openSDA in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Use-segger-J-link-instead-of-openSDA/m-p/722860#M1462</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Within simulink i can select a com port or openSDA to download code to the target. Is it possible to use a J-link from Segger for this purpose?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Apr 2018 07:28:06 GMT</pubDate>
    <dc:creator>theopubben</dc:creator>
    <dc:date>2018-04-11T07:28:06Z</dc:date>
    <item>
      <title>Use segger J-link instead of openSDA</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Use-segger-J-link-instead-of-openSDA/m-p/722860#M1462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Within simulink i can select a com port or openSDA to download code to the target. Is it possible to use a J-link from Segger for this purpose?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 07:28:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Use-segger-J-link-instead-of-openSDA/m-p/722860#M1462</guid>
      <dc:creator>theopubben</dc:creator>
      <dc:date>2018-04-11T07:28:06Z</dc:date>
    </item>
    <item>
      <title>Re: Use segger J-link instead of openSDA</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Use-segger-J-link-instead-of-openSDA/m-p/722861#M1463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Theo,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Simulink can only download (for the moment) via UART type protocols. Hence you cannot use JTAG based protocols directly from Simulink - BUT - you may generate and built the application from Simulink and get the elf/mot/srec file associated with the application and downloaded via the J-link using an external debugger such as S32 Design Studio that support the JTAG based protocols.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Apr 2018 09:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Use-segger-J-link-instead-of-openSDA/m-p/722861#M1463</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2018-04-11T09:04:02Z</dc:date>
    </item>
  </channel>
</rss>