<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: Programming the simulink generated code onto the hardware using JTAG</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Programming-the-simulink-generated-code-onto-the-hardware-using/m-p/696552#M1106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to install RappID_BL on my PC but I get "Error 1721". It has to do with the windows installer but I am not completely sure how to overcome the error. I will try to run this once I successfully install the software. Thank you for the answer though :smileyhappy:&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Sep 2017 08:54:09 GMT</pubDate>
    <dc:creator>raghurajappa</dc:creator>
    <dc:date>2017-09-19T08:54:09Z</dc:date>
    <item>
      <title>Programming the simulink generated code onto the hardware using JTAG</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Programming-the-simulink-generated-code-onto-the-hardware-using/m-p/696550#M1104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have created simulink models and generated C code too, for MPC5744L microcontroller which is connected to a daughter board and eventually to the XPC56XX B rev motherboard. This program is a simple LED + Button configuration.&lt;/P&gt;&lt;P&gt;Now the next step is to program this generated code directly onto the hardware to see the LED blink with button clicks. But I am stuck at this step because I could not find a step by step tutorial showing me how to program the hardware using the JTAG pins (I currently use a PLS-USB JTAG debugger). I could however find a video that shows how I can flash the code using FreeMaster and serial communication. But I intend to use the JTAG debugger and do not know how to integrate PLS software with Simulink such that the integration works seamelessly to program the generated code onto the hardware.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help/suggestions is appreciated.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary - I have MATLAB generated code and want to use the JTAG connection to program the hardware. I am stuck because i do not know how to do this (couldn't find a tutorial/step-by-step guide).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you :smileyhappy:&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Sep 2017 11:50:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Programming-the-simulink-generated-code-onto-the-hardware-using/m-p/696550#M1104</guid>
      <dc:creator>raghurajappa</dc:creator>
      <dc:date>2017-09-07T11:50:52Z</dc:date>
    </item>
    <item>
      <title>Re: Programming the simulink generated code onto the hardware using JTAG</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Programming-the-simulink-generated-code-onto-the-hardware-using/m-p/696551#M1105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/raghurajappa"&gt;raghurajappa&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our RAppID_BL.exe application that is called of the end of the building process to write the elf into the target supports only UART or CAN interfaces.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30313i64B1C754912B8172/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If none of the above are interface are missing from your board setup then you might be able to modify the mfile that calls the RAppID_BL.exe and instead of executing the NXP's application you may call your own IDE/utility/cmd tool that should take the elf and program if via the JTAG using your own probe into the target. That might work fine for your use case but for sure it will not works for PIL simulations since there is a much more complex communication protocol in place to communicate with the HW.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Sep 2017 15:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Programming-the-simulink-generated-code-onto-the-hardware-using/m-p/696551#M1105</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2017-09-08T15:06:51Z</dc:date>
    </item>
    <item>
      <title>Re: Programming the simulink generated code onto the hardware using JTAG</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Programming-the-simulink-generated-code-onto-the-hardware-using/m-p/696552#M1106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to install RappID_BL on my PC but I get "Error 1721". It has to do with the windows installer but I am not completely sure how to overcome the error. I will try to run this once I successfully install the software. Thank you for the answer though :smileyhappy:&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2017 08:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Programming-the-simulink-generated-code-onto-the-hardware-using/m-p/696552#M1106</guid>
      <dc:creator>raghurajappa</dc:creator>
      <dc:date>2017-09-19T08:54:09Z</dc:date>
    </item>
    <item>
      <title>Re: Programming the simulink generated code onto the hardware using JTAG</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Programming-the-simulink-generated-code-onto-the-hardware-using/m-p/696553#M1107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RappID_BL is delivered with the Motor Control Toolbox for MPC564xL.&lt;/P&gt;&lt;P&gt;You can find it in C:\MCToolbox\rappid564xl\tools\BootLoader.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2017 09:14:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Programming-the-simulink-generated-code-onto-the-hardware-using/m-p/696553#M1107</guid>
      <dc:creator>paulvlase</dc:creator>
      <dc:date>2017-09-19T09:14:08Z</dc:date>
    </item>
  </channel>
</rss>