<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックMCSPTE1AK144 – Motor Faults Immediately After Starting MATLAB Host Model</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MCSPTE1AK144-Motor-Faults-Immediately-After-Starting-MATLAB-Host/m-p/2418418#M10828</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I am facing an issue while controlling the MCSPTE1AK144 kit using the MATLAB/Simulink open-loop and closed loop examples available.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The target model builds and the generated &lt;/SPAN&gt;&lt;SPAN&gt;file can be flashed to the S32K144 successfully. MATLAB also detects the OpenSDA CDC serial port and the host model is able to establish communication.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, whenever I start the host model and switch the motor ON, the motor shaft either twitches briefly or does not run, and the D11 red LED immediately turns ON/flashes, indicating a fault. The motor then stops responding.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Basic board communication has been verified separately using the LPUART Hello World example, which builds, flashes, and communicates successfully through the OpenSDA serial port.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you please advise what could cause the motor-control application to enter a fault immediately after starting control from the MATLAB host model, and which fault/status variables should be checked to identify the root cause?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hardware: MCSPTE1AK144 (S32K144-EVB + DEVKIT-MOTORGD)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Motor: Sunrise 42BLY3A78-24110&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MATLAB/Simulink with NXP MBDT&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 05 Oct 2026 10:36:18 GMT</pubDate>
    <dc:creator>Thishal</dc:creator>
    <dc:date>2026-10-05T10:36:18Z</dc:date>
    <item>
      <title>MCSPTE1AK144 – Motor Faults Immediately After Starting MATLAB Host Model</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MCSPTE1AK144-Motor-Faults-Immediately-After-Starting-MATLAB-Host/m-p/2418418#M10828</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am facing an issue while controlling the MCSPTE1AK144 kit using the MATLAB/Simulink open-loop and closed loop examples available.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The target model builds and the generated &lt;/SPAN&gt;&lt;SPAN&gt;file can be flashed to the S32K144 successfully. MATLAB also detects the OpenSDA CDC serial port and the host model is able to establish communication.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, whenever I start the host model and switch the motor ON, the motor shaft either twitches briefly or does not run, and the D11 red LED immediately turns ON/flashes, indicating a fault. The motor then stops responding.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Basic board communication has been verified separately using the LPUART Hello World example, which builds, flashes, and communicates successfully through the OpenSDA serial port.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you please advise what could cause the motor-control application to enter a fault immediately after starting control from the MATLAB host model, and which fault/status variables should be checked to identify the root cause?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hardware: MCSPTE1AK144 (S32K144-EVB + DEVKIT-MOTORGD)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Motor: Sunrise 42BLY3A78-24110&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MATLAB/Simulink with NXP MBDT&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Oct 2026 10:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MCSPTE1AK144-Motor-Faults-Immediately-After-Starting-MATLAB-Host/m-p/2418418#M10828</guid>
      <dc:creator>Thishal</dc:creator>
      <dc:date>2026-10-05T10:36:18Z</dc:date>
    </item>
  </channel>
</rss>