<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K358 MBDT/Simulink – Store SOC in Non-Volatile Memory in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-MBDT-Simulink-Store-SOC-in-Non-Volatile-Memory/m-p/2416449#M10826</link>
    <description>&lt;P&gt;Hello NXP Team,&lt;BR /&gt;I am using the RD-BESSK358BMU board (S32K358 MCU) with MATLAB/Simulink and NXP MBDT.&lt;BR /&gt;I have an EKF SOC estimator running on the board. I need to periodically save the calculated SOC in non-volatile memory, so after a complete power OFF/ON, the last stored SOC can be read and used as the initial SOC of the EKF.&lt;BR /&gt;What is the recommended way to implement this in Simulink/MBDT for S32K358?&lt;BR /&gt;I can see Fee, MemAcc, and Mem_43_InFls in the S32 Configuration Tool. Should these modules be used for this purpose?&lt;BR /&gt;Is there any S32K358 Simulink/MBDT example for non-volatile Read/Write that you can share?&lt;BR /&gt;I found older S32K examples using EEPROM/FEE, but I am specifically looking for the recommended solution for S32K358 with Simulink/MBDT.&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Sat, 26 Sep 2026 09:11:36 GMT</pubDate>
    <dc:creator>samansaki</dc:creator>
    <dc:date>2026-09-26T09:11:36Z</dc:date>
    <item>
      <title>S32K358 MBDT/Simulink – Store SOC in Non-Volatile Memory</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-MBDT-Simulink-Store-SOC-in-Non-Volatile-Memory/m-p/2416449#M10826</link>
      <description>&lt;P&gt;Hello NXP Team,&lt;BR /&gt;I am using the RD-BESSK358BMU board (S32K358 MCU) with MATLAB/Simulink and NXP MBDT.&lt;BR /&gt;I have an EKF SOC estimator running on the board. I need to periodically save the calculated SOC in non-volatile memory, so after a complete power OFF/ON, the last stored SOC can be read and used as the initial SOC of the EKF.&lt;BR /&gt;What is the recommended way to implement this in Simulink/MBDT for S32K358?&lt;BR /&gt;I can see Fee, MemAcc, and Mem_43_InFls in the S32 Configuration Tool. Should these modules be used for this purpose?&lt;BR /&gt;Is there any S32K358 Simulink/MBDT example for non-volatile Read/Write that you can share?&lt;BR /&gt;I found older S32K examples using EEPROM/FEE, but I am specifically looking for the recommended solution for S32K358 with Simulink/MBDT.&lt;BR /&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Sat, 26 Sep 2026 09:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-MBDT-Simulink-Store-SOC-in-Non-Volatile-Memory/m-p/2416449#M10826</guid>
      <dc:creator>samansaki</dc:creator>
      <dc:date>2026-09-26T09:11:36Z</dc:date>
    </item>
  </channel>
</rss>