<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Random occurences of timeouts while reading variables in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Random-occurences-of-timeouts-while-reading-variables/m-p/2398395#M10783</link>
    <description>&lt;P&gt;Hello, I have been working on a battery test rig set up by my predecessors on the project.&lt;BR /&gt;The test rig uses an nxp S32K144EVB board connected via usb to a computer.&lt;/P&gt;&lt;P&gt;The code is built from a simulink file and monitoring of the test is made via FreeMASTER 3.2.&lt;/P&gt;&lt;P&gt;The project has been working on a laptop for a few months and it has been necessary to configure a new laptop as a replacement. However, even while installing the same FreeMASTER version, the same drivers and using the same project files, all variable reads as "?" due to timeout errors after a seemingly random duration.&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Logged errors after 12 minutes of runtime with no issues :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fbw_0-1784820901163.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393087iB91AADD15F6E20F0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="fbw_0-1784820901163.png" alt="fbw_0-1784820901163.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fbw_0-1784820901163.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 23 Jul 2026 15:39:38 GMT</pubDate>
    <dc:creator>fbw</dc:creator>
    <dc:date>2026-07-23T15:39:38Z</dc:date>
    <item>
      <title>Random occurences of timeouts while reading variables</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Random-occurences-of-timeouts-while-reading-variables/m-p/2398395#M10783</link>
      <description>&lt;P&gt;Hello, I have been working on a battery test rig set up by my predecessors on the project.&lt;BR /&gt;The test rig uses an nxp S32K144EVB board connected via usb to a computer.&lt;/P&gt;&lt;P&gt;The code is built from a simulink file and monitoring of the test is made via FreeMASTER 3.2.&lt;/P&gt;&lt;P&gt;The project has been working on a laptop for a few months and it has been necessary to configure a new laptop as a replacement. However, even while installing the same FreeMASTER version, the same drivers and using the same project files, all variable reads as "?" due to timeout errors after a seemingly random duration.&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Logged errors after 12 minutes of runtime with no issues :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fbw_0-1784820901163.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/393087iB91AADD15F6E20F0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="fbw_0-1784820901163.png" alt="fbw_0-1784820901163.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;fbw_0-1784820901163.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jul 2026 15:39:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Random-occurences-of-timeouts-while-reading-variables/m-p/2398395#M10783</guid>
      <dc:creator>fbw</dc:creator>
      <dc:date>2026-07-23T15:39:38Z</dc:date>
    </item>
    <item>
      <title>Re: Random occurences of timeouts while reading variables</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Random-occurences-of-timeouts-while-reading-variables/m-p/2404290#M10794</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I don't think I encounter that problem yet but I have a few suggestions, maybe they can help:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Try to power up the S32K144EVB from a 12V power supply instead from the USB.&amp;nbsp;&lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-s32k144evb:NGS-S32K144EVB?section=out-of-the-box" target="_blank" rel="noopener"&gt;Getting Started with the S32K144EVB&lt;/A&gt;&amp;nbsp;&lt;/LI&gt;
&lt;LI&gt;Try different methods to connect the FreeMASTER project to the EVB:
&lt;UL&gt;
&lt;LI&gt;Use the onboard USB connector&lt;/LI&gt;
&lt;LI&gt;External Serial2USB convertor&lt;/LI&gt;
&lt;LI&gt;Use a debug probe to connect directly to the S32K144 MCU&lt;/LI&gt;
&lt;/UL&gt;
&lt;/LI&gt;
&lt;LI&gt;Try to reduce the refresh time for non critical variables&lt;/LI&gt;
&lt;LI&gt;Prevent the laptop to enter sleep mode (as it might cut USB power to save battery).&lt;/LI&gt;
&lt;LI&gt;Try to create a new FreeMASTER project from scratch.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Sorin Bancila&lt;/P&gt;</description>
      <pubDate>Wed, 12 Aug 2026 15:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Random-occurences-of-timeouts-while-reading-variables/m-p/2404290#M10794</guid>
      <dc:creator>SorinIBancila</dc:creator>
      <dc:date>2026-08-12T15:19:47Z</dc:date>
    </item>
  </channel>
</rss>