<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 Re: S32K1 Toolbox - Latest version of MATLAB that is compatible</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2372421#M10768</link>
    <description>&lt;P&gt;Hey&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180247"&gt;@SorinIBancila&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you manage to find out about the EEPROM blocks by any chance? Thank you!&lt;/P&gt;</description>
    <pubDate>Thu, 28 May 2026 10:44:32 GMT</pubDate>
    <dc:creator>Poley</dc:creator>
    <dc:date>2026-05-28T10:44:32Z</dc:date>
    <item>
      <title>S32K1 Toolbox - Latest version of MATLAB that is compatible</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2370104#M10752</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am setting up a new laptop and need to move all of my prvious models and projects over to a fresh install. I am installing MATLAB, obviously I would rather use the latest version possible but what is the latest MATLAB version the MBDT toolbox works with? I would assume it will work with any but a set release is specified as this is what the toolbox was tested with?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 08:36:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2370104#M10752</guid>
      <dc:creator>Poley</dc:creator>
      <dc:date>2026-05-22T08:36:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1 Toolbox - Latest version of MATLAB that is compatible</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2370115#M10753</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The toolbox should work with all new versions but you should take it with a grain of salt because the toolbox was not tested on these version (R2023a+) as they were not available back then.&lt;/P&gt;
&lt;P&gt;I would recommend to stick to R2022a (the latest official version supported) if it is possible.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Sorin Bancila&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 08:47:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2370115#M10753</guid>
      <dc:creator>SorinIBancila</dc:creator>
      <dc:date>2026-05-22T08:47:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1 Toolbox - Latest version of MATLAB that is compatible</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2370124#M10755</link>
      <description>&lt;P&gt;Hey Sorin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No problem, thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, is there an easy way to transfer my toolbox over or do I need to start fresh? Just as I have multiple patches applied mainly from conversations with Marius. If it needs to be a fresh install then no problem, I can go through and find them again.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Lastly, while talking about patches. I was wondering if it is possible to make the offset in the flash EERead or EEwrite blocks to be an input instead of a set value in the block config? Is this something easily modified on my end by modifying the mask or would it require another patch to change? Just as I have a cyclic memory write for SOC that makes use of 40 different address sets to preserve EEPROM life. It would greatly reduce my model if I could modify the offset with a single value instead of using multiple subsystems if that makes sense?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Thanks again!&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 08:56:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2370124#M10755</guid>
      <dc:creator>Poley</dc:creator>
      <dc:date>2026-05-22T08:56:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1 Toolbox - Latest version of MATLAB that is compatible</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2370141#M10758</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no official way to migrate toolbox from one computer to another. One solution that MIGHT work would be to go to the addons folder in MATLAB and copy-paste the entire toolbox on the new computer in the addons folder. Then, I recommend to run the &lt;STRONG&gt;mbd_s32k1_path&lt;/STRONG&gt; to make sure everything is in path. Please make sure you generate a new license file for the new laptop.&lt;/P&gt;
&lt;P&gt;Important! Before trying these, please make sure you have backup in case something fails.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regarding the issue about EERead, EEwrite, I don't know yet. Let me investigate and I will come back with an anwser.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Sorin Bancila&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 09:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2370141#M10758</guid>
      <dc:creator>SorinIBancila</dc:creator>
      <dc:date>2026-05-22T09:18:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32K1 Toolbox - Latest version of MATLAB that is compatible</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2372421#M10768</link>
      <description>&lt;P&gt;Hey&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180247"&gt;@SorinIBancila&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Did you manage to find out about the EEPROM blocks by any chance? Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 28 May 2026 10:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K1-Toolbox-Latest-version-of-MATLAB-that-is-compatible/m-p/2372421#M10768</guid>
      <dc:creator>Poley</dc:creator>
      <dc:date>2026-05-28T10:44:32Z</dc:date>
    </item>
  </channel>
</rss>