<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Board recommendation for MBDT BMS development + edge AI inference on NXP hardware in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Board-recommendation-for-MBDT-BMS-development-edge-AI-inference/m-p/2361241#M10747</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;Sorin,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much for your detailed reply.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to clarify my use case further. My work does not require live battery cell measurement through an AFE chip — I am using dataset replay over CAN FD. Therefore I believe I only need the MBDT for S32K3 (general codegen toolbox), not the MBDT for BMS add-on. The official MBDT for S32K3 documentation lists the S32K3X4EVB-T172 as a validated board. Could you confirm whether the S32K3X4EVB-T172 is appropriate for: Simulink model deployment via Embedded Coder, SIL/PIL validation, FreeMASTER data logging, and CAN FD communication — without requiring any AFE cell controller integration? If so, this board seems to meet all my work requirements without the complexity of the HVBMS reference kits.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Additionally, I plan to connect the S32K3X4EVB-T172 to a second NXP evaluation board — preferably something among MCXN947 series (eIQ Neutron NPU) — via CAN FD. The S32K3X4EVB-T172 would act as the BMS controller sending data and the MCXN947 board would receive them and run neural network inference on its NPU. Both boards appear to have on-board CAN FD transceivers. Could you confirm whether a direct 3-wire CAN FD connection (CANH, CANL, GND) between these two boards is feasible on a short bench cable, and whether any termination resistors or jumper configuration is required on either board for this setup?&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For the NPU based inference side of my work, I have looked at the MCX-N9XX-EVK. My work requires: INT8 quantized TF Lite model deployment via the eIQ toolkit, real-time CAN FD data reception, NPU inference latency measurement and power consumption measurement during NPU inference to report energy per inference. Is this evaluation board best suitable for my work?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please also recommend other boards apart from two I mentioned when they are more suitable for my work. As mentioned by you regarding the edge AI boards, if possible, could you please point my query to the concerned&amp;nbsp; person from your team?&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I hope my detailed explanation helps you and please let me know for more information when needed. Thank you very much again for your time and guidance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Miraj&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 06 May 2026 13:56:10 GMT</pubDate>
    <dc:creator>miraj</dc:creator>
    <dc:date>2026-05-06T13:56:10Z</dc:date>
    <item>
      <title>Board recommendation for MBDT BMS development + edge AI inference on NXP hardware</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Board-recommendation-for-MBDT-BMS-development-edge-AI-inference/m-p/2359267#M10731</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello NXP Team,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on combining two NXP-based development streams:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;**Stream 1 — Model-based BMS development:**&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Using MATLAB/Simulink with Embedded Coder and the Model-Based Design Toolbox for S32K3, I need to deploy a Battery Management System model as generated C code on an NXP S32K3-series microcontroller. The key requirements are: full MBDT for S32K3 support, SIL/PIL/External mode validation, FreeMASTER data logging, CAN FD interface, and ASIL D functional safety rating. I have been briefly looking at the S32K344 family as the target MCU.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;**Stream 2 — Edge AI inference:**&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Alongside the BMS controller, I need a second NXP board running quantized INT8 neural network models (TCN architecture, TF Lite format) on an NPU for real-time SOC estimation and short-horizon temperature prediction. I have been looking at the MCX N947-based boards for this purpose given the eIQ Neutron NPU.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;**My questions:**&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Given these two requirements, which specific NXP development boards would you recommend for each stream? I have done some research and have two or three boards in mind for the S32K344 side, but would highly prefer and value your recommendation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2. For the edge AI board, is the MCX-N9XX-EVK or the FRDM-MCXN947 more appropriate for a context where I also want to measure power consumption during NPU inference?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3. Can the recommended boards communicate directly over CAN FD with a simple 3-wire bench connection, or is additional hardware required?&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; I hope my details are sufficient. If you need more information, please let me know. Thank you very much in advance for your guidance and time.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 30 Apr 2026 10:55:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Board-recommendation-for-MBDT-BMS-development-edge-AI-inference/m-p/2359267#M10731</guid>
      <dc:creator>miraj</dc:creator>
      <dc:date>2026-04-30T10:55:59Z</dc:date>
    </item>
    <item>
      <title>Re: Board recommendation for MBDT BMS development + edge AI inference on NXP hardware</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Board-recommendation-for-MBDT-BMS-development-edge-AI-inference/m-p/2360997#M10734</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;1. The recommended hardware for the Model Based Design Toolbox for BMS are the &lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/RD-K344BMU" target="_self"&gt;400V HVBMS S32K344&lt;/A&gt;&amp;nbsp;and the &lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/RD-K358BMU" target="_self"&gt;800V HVBMS S32K358&lt;/A&gt;. I would pick the hardware based on architecture required (400V vs 800V). Both of them are well supported in the toolbox, with various examples.&lt;/P&gt;
&lt;P&gt;2. Unfortunately, these boards are not supported by any toolbox we provide. I don't have any experience with these boards, so I can't really recommend one.&lt;/P&gt;
&lt;P&gt;3. The hardware needed for CAN communication usually consist of two components:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;CAN Controller: For S32K344, S32K358, it is included in the chip itself.&lt;/LI&gt;
&lt;LI&gt;CAN Transceiver: For evaluation boards for S32K344, S32K358, it is an external IC (TJA1043, TJA1145 etc) which is mounted on the evaluation board.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Most of the evaluation boards include all the required hardware for CAN, but I recommend you to check these before buying.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Sorin Bancila&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 May 2026 08:15:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Board-recommendation-for-MBDT-BMS-development-edge-AI-inference/m-p/2360997#M10734</guid>
      <dc:creator>SorinIBancila</dc:creator>
      <dc:date>2026-05-06T08:15:44Z</dc:date>
    </item>
    <item>
      <title>Re: Board recommendation for MBDT BMS development + edge AI inference on NXP hardware</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Board-recommendation-for-MBDT-BMS-development-edge-AI-inference/m-p/2361241#M10747</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;Sorin,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you very much for your detailed reply.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would like to clarify my use case further. My work does not require live battery cell measurement through an AFE chip — I am using dataset replay over CAN FD. Therefore I believe I only need the MBDT for S32K3 (general codegen toolbox), not the MBDT for BMS add-on. The official MBDT for S32K3 documentation lists the S32K3X4EVB-T172 as a validated board. Could you confirm whether the S32K3X4EVB-T172 is appropriate for: Simulink model deployment via Embedded Coder, SIL/PIL validation, FreeMASTER data logging, and CAN FD communication — without requiring any AFE cell controller integration? If so, this board seems to meet all my work requirements without the complexity of the HVBMS reference kits.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Additionally, I plan to connect the S32K3X4EVB-T172 to a second NXP evaluation board — preferably something among MCXN947 series (eIQ Neutron NPU) — via CAN FD. The S32K3X4EVB-T172 would act as the BMS controller sending data and the MCXN947 board would receive them and run neural network inference on its NPU. Both boards appear to have on-board CAN FD transceivers. Could you confirm whether a direct 3-wire CAN FD connection (CANH, CANL, GND) between these two boards is feasible on a short bench cable, and whether any termination resistors or jumper configuration is required on either board for this setup?&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For the NPU based inference side of my work, I have looked at the MCX-N9XX-EVK. My work requires: INT8 quantized TF Lite model deployment via the eIQ toolkit, real-time CAN FD data reception, NPU inference latency measurement and power consumption measurement during NPU inference to report energy per inference. Is this evaluation board best suitable for my work?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please also recommend other boards apart from two I mentioned when they are more suitable for my work. As mentioned by you regarding the edge AI boards, if possible, could you please point my query to the concerned&amp;nbsp; person from your team?&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I hope my detailed explanation helps you and please let me know for more information when needed. Thank you very much again for your time and guidance.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Miraj&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 06 May 2026 13:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Board-recommendation-for-MBDT-BMS-development-edge-AI-inference/m-p/2361241#M10747</guid>
      <dc:creator>miraj</dc:creator>
      <dc:date>2026-05-06T13:56:10Z</dc:date>
    </item>
    <item>
      <title>Re: Board recommendation for MBDT BMS development + edge AI inference on NXP hardware</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Board-recommendation-for-MBDT-BMS-development-edge-AI-inference/m-p/2370147#M10760</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;1. Yes, S32K3X4EVB-T172 is suitable for your application and I don't see any reasons why it can't fulfill your requirements. We provide example for each subject you said (sil/pil, freemaster logging, CAN) and I recommend you to check them first. Make sure you install the latest S32K3 toolbox in this case (1.8.0).&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2. I am pretty sure that you can connect these 2 boards together via CAN FD without any extra hardware setup (such as resistors). About the jumpers, you have to check out the Quick Start Guide/Schematics for each board, to make sure the headers are connected onboard to the CAN pins.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;3. I will try to ask around about the MCX-N9XX-EVK but I can't guarantee that I can help you on this.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Sorin Bancila&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 May 2026 09:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Board-recommendation-for-MBDT-BMS-development-edge-AI-inference/m-p/2370147#M10760</guid>
      <dc:creator>SorinIBancila</dc:creator>
      <dc:date>2026-05-22T09:24:52Z</dc:date>
    </item>
  </channel>
</rss>