<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックErrors Deploying Examples to iMX RT1170 EVKB Evaluation Kit</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Errors-Deploying-Examples-to-iMX-RT1170-EVKB-Evaluation-Kit/m-p/2325938#M10663</link>
    <description>&lt;P&gt;I am trying to use NXP’s Model Based Design Toolbox to quickly deploy an existing design to an i.MX RT1170-EVKB Evaluation Kit. I have collected what I believe to be the totality of the stack required to achieve this and to verify that it is all working properly I would like to deploy one of the examples that comes with it. (For clarity I have already deployed an example using the SDK directly.) I have chosen the “evkmimxrt1170_gpio_interrupt” as the example to model to deploy. In trying to deploy the model the first issue I encounter is with the model check failing with “Dot indexing is not supported for variables of this type.” If I bypass the model checks I receive a “Failure in generate_configuration_code(0) : MEX code generation: Failed to generate configuration files” which then inline with expectation gives complaints in compile about missing includes.&lt;/P&gt;</description>
    <pubDate>Wed, 04 Mar 2026 04:40:49 GMT</pubDate>
    <dc:creator>gmt</dc:creator>
    <dc:date>2026-03-04T04:40:49Z</dc:date>
    <item>
      <title>Errors Deploying Examples to iMX RT1170 EVKB Evaluation Kit</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Errors-Deploying-Examples-to-iMX-RT1170-EVKB-Evaluation-Kit/m-p/2325938#M10663</link>
      <description>&lt;P&gt;I am trying to use NXP’s Model Based Design Toolbox to quickly deploy an existing design to an i.MX RT1170-EVKB Evaluation Kit. I have collected what I believe to be the totality of the stack required to achieve this and to verify that it is all working properly I would like to deploy one of the examples that comes with it. (For clarity I have already deployed an example using the SDK directly.) I have chosen the “evkmimxrt1170_gpio_interrupt” as the example to model to deploy. In trying to deploy the model the first issue I encounter is with the model check failing with “Dot indexing is not supported for variables of this type.” If I bypass the model checks I receive a “Failure in generate_configuration_code(0) : MEX code generation: Failed to generate configuration files” which then inline with expectation gives complaints in compile about missing includes.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Mar 2026 04:40:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Errors-Deploying-Examples-to-iMX-RT1170-EVKB-Evaluation-Kit/m-p/2325938#M10663</guid>
      <dc:creator>gmt</dc:creator>
      <dc:date>2026-03-04T04:40:49Z</dc:date>
    </item>
    <item>
      <title>Re: Errors Deploying Examples to iMX RT1170 EVKB Evaluation Kit</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Errors-Deploying-Examples-to-iMX-RT1170-EVKB-Evaluation-Kit/m-p/2351237#M10713</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Can you describe the steps you took to make it work? What MATLAB do you use? What IMXRT toolbox version did you install?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I've tried on a fresh toolbox installation in MATLAB R2024b and R2025b. I was able to generate the code for the&amp;nbsp;evkmimxrt1170_gpio_interrupt example without any change.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Sorin Bancila&lt;/P&gt;</description>
      <pubDate>Wed, 15 Apr 2026 08:41:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Errors-Deploying-Examples-to-iMX-RT1170-EVKB-Evaluation-Kit/m-p/2351237#M10713</guid>
      <dc:creator>SorinIBancila</dc:creator>
      <dc:date>2026-04-15T08:41:08Z</dc:date>
    </item>
  </channel>
</rss>