<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Adc Hw Unit Group In ADC_BUSY state in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Adc-Hw-Unit-Group-In-ADC-BUSY-state/m-p/2324460#M10661</link>
    <description>&lt;P&gt;Hi NXP Team.&lt;/P&gt;&lt;P&gt;I'm using MDBT ina&amp;nbsp;&lt;SPAN&gt;S&lt;/SPAN&gt;&lt;SPAN&gt;32k358 custom board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm facing problems with the ADC HW units.&lt;/P&gt;&lt;P&gt;In my configuration i have 2 ADC1 groups: one with 10 channels and the other with 3 channels.&lt;/P&gt;&lt;P&gt;The group with 10 ch is converted every 800us, while the 3 ch group conversion is called inside emios callback triggered with both rising and trailing edge of a PWM signal, which has a fixed period of 200Hz (so there are 2 ADC coversion close together, based on the duty value).&lt;/P&gt;&lt;P&gt;When i try to modify the duty cycle of the PWM i've found that the 10ch group become ADC_BUSY and doesn't recover anymore.&lt;/P&gt;&lt;P&gt;I've found this problem also in older project with more groups per ADC Hw unit, which the conversions started every 10ms and, after some time, the majority of them become ADC_BUSY without recovering anymore.&lt;/P&gt;&lt;P&gt;Also adc queue is/was enabled at 1024 elements.&lt;/P&gt;&lt;P&gt;Could anybody help me understand this?&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Simon&lt;/P&gt;</description>
    <pubDate>Fri, 27 Feb 2026 16:13:20 GMT</pubDate>
    <dc:creator>simon98</dc:creator>
    <dc:date>2026-02-27T16:13:20Z</dc:date>
    <item>
      <title>Adc Hw Unit Group In ADC_BUSY state</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Adc-Hw-Unit-Group-In-ADC-BUSY-state/m-p/2324460#M10661</link>
      <description>&lt;P&gt;Hi NXP Team.&lt;/P&gt;&lt;P&gt;I'm using MDBT ina&amp;nbsp;&lt;SPAN&gt;S&lt;/SPAN&gt;&lt;SPAN&gt;32k358 custom board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm facing problems with the ADC HW units.&lt;/P&gt;&lt;P&gt;In my configuration i have 2 ADC1 groups: one with 10 channels and the other with 3 channels.&lt;/P&gt;&lt;P&gt;The group with 10 ch is converted every 800us, while the 3 ch group conversion is called inside emios callback triggered with both rising and trailing edge of a PWM signal, which has a fixed period of 200Hz (so there are 2 ADC coversion close together, based on the duty value).&lt;/P&gt;&lt;P&gt;When i try to modify the duty cycle of the PWM i've found that the 10ch group become ADC_BUSY and doesn't recover anymore.&lt;/P&gt;&lt;P&gt;I've found this problem also in older project with more groups per ADC Hw unit, which the conversions started every 10ms and, after some time, the majority of them become ADC_BUSY without recovering anymore.&lt;/P&gt;&lt;P&gt;Also adc queue is/was enabled at 1024 elements.&lt;/P&gt;&lt;P&gt;Could anybody help me understand this?&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Simon&lt;/P&gt;</description>
      <pubDate>Fri, 27 Feb 2026 16:13:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Adc-Hw-Unit-Group-In-ADC-BUSY-state/m-p/2324460#M10661</guid>
      <dc:creator>simon98</dc:creator>
      <dc:date>2026-02-27T16:13:20Z</dc:date>
    </item>
  </channel>
</rss>