<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックS32K358 ASIL Compliant Architecture Using MBDT</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-ASIL-Compliant-Architecture-Using-MBDT/m-p/2324423#M10660</link>
    <description>&lt;P&gt;I am currently in development of a system using the S32K358 with MBDT in Simulink with the intent of supporting the ASIL capability of the chip.&lt;/P&gt;&lt;P&gt;I have been able to deploy my model on the S32K on a single core and in order to align with the ASIL capability of the chip I want to understand how to architecture the system and model to run on multiple cores.&lt;BR /&gt;The model has been architected such that it is split into 2 sections, the 'safety' layer which would be deployed on the ASIL D capable lockstep core, and the 'application' layer on the other core.&lt;/P&gt;&lt;P&gt;From reading some info on the community page there doesn't appear to be multicore support using MBDT for the S32K. Can you confirm if this is the case?&lt;/P&gt;&lt;P&gt;If not can you provide some insight into the best approach, for example would I have to develop the 'safety' layer using your S32DS whilst keeping the application code in Simulink?&lt;BR /&gt;I imagine this would need additional consideration for code generation, flashing and management of multiple files and MiL testing in the simulink environment.&lt;/P&gt;&lt;P&gt;As a follow up question, the application needs to be aware of the safety element and read various signals. What is the approach for intercore communication? Would there need to be a shared memory area that both cores can access and can this be managed using MBDT.&lt;/P&gt;&lt;P&gt;For reference I am currently using S32K3 1.4.0 and BMS 1.2.0 MBDT toolboxes.&lt;/P&gt;&lt;P&gt;Thanks for the support.&lt;/P&gt;</description>
    <pubDate>Fri, 27 Feb 2026 13:25:03 GMT</pubDate>
    <dc:creator>OllieSaunders</dc:creator>
    <dc:date>2026-02-27T13:25:03Z</dc:date>
    <item>
      <title>S32K358 ASIL Compliant Architecture Using MBDT</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-ASIL-Compliant-Architecture-Using-MBDT/m-p/2324423#M10660</link>
      <description>&lt;P&gt;I am currently in development of a system using the S32K358 with MBDT in Simulink with the intent of supporting the ASIL capability of the chip.&lt;/P&gt;&lt;P&gt;I have been able to deploy my model on the S32K on a single core and in order to align with the ASIL capability of the chip I want to understand how to architecture the system and model to run on multiple cores.&lt;BR /&gt;The model has been architected such that it is split into 2 sections, the 'safety' layer which would be deployed on the ASIL D capable lockstep core, and the 'application' layer on the other core.&lt;/P&gt;&lt;P&gt;From reading some info on the community page there doesn't appear to be multicore support using MBDT for the S32K. Can you confirm if this is the case?&lt;/P&gt;&lt;P&gt;If not can you provide some insight into the best approach, for example would I have to develop the 'safety' layer using your S32DS whilst keeping the application code in Simulink?&lt;BR /&gt;I imagine this would need additional consideration for code generation, flashing and management of multiple files and MiL testing in the simulink environment.&lt;/P&gt;&lt;P&gt;As a follow up question, the application needs to be aware of the safety element and read various signals. What is the approach for intercore communication? Would there need to be a shared memory area that both cores can access and can this be managed using MBDT.&lt;/P&gt;&lt;P&gt;For reference I am currently using S32K3 1.4.0 and BMS 1.2.0 MBDT toolboxes.&lt;/P&gt;&lt;P&gt;Thanks for the support.&lt;/P&gt;</description>
      <pubDate>Fri, 27 Feb 2026 13:25:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-ASIL-Compliant-Architecture-Using-MBDT/m-p/2324423#M10660</guid>
      <dc:creator>OllieSaunders</dc:creator>
      <dc:date>2026-02-27T13:25:03Z</dc:date>
    </item>
  </channel>
</rss>