<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックIssue with CAN Communication using NXP Controller and MBDT on MATLAB</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-with-CAN-Communication-using-NXP-Controller-and-MBDT-on/m-p/2301789#M10612</link>
    <description>&lt;DIV class=""&gt;&lt;P&gt;We are working on a VCU that has&amp;nbsp;NXP&amp;nbsp;S32K144 controller platform.&lt;/P&gt;&lt;P&gt;We are facing issues receiving and transmitting CAN messages using&amp;nbsp;NXP&amp;nbsp;Support Package on MATLAB for this controller.&lt;/P&gt;&lt;P&gt;While we can Rx CAN message if a dedicated "Message Buffer" is provided for each ID in "FCAN_Receive" block settings, but this is not a ideal solution. The number of "Message Buffer" has a limit of 15. So we could not have dedicated message buffer for each Rx message if we have more than 15 messages.&lt;/P&gt;&lt;P&gt;We have quite a lot of CAN IDs to send and receive on bus and hence would need a mask to receive multiple IDs with same "Message Buffer". We tried using mask but that is not working for us.&lt;/P&gt;&lt;P&gt;We could not receive messages properly, if we put a common "Message Buffer" and some ID mask.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;</description>
    <pubDate>Wed, 28 Jan 2026 04:45:12 GMT</pubDate>
    <dc:creator>ashutoshsahu</dc:creator>
    <dc:date>2026-01-28T04:45:12Z</dc:date>
    <item>
      <title>Issue with CAN Communication using NXP Controller and MBDT on MATLAB</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-with-CAN-Communication-using-NXP-Controller-and-MBDT-on/m-p/2301789#M10612</link>
      <description>&lt;DIV class=""&gt;&lt;P&gt;We are working on a VCU that has&amp;nbsp;NXP&amp;nbsp;S32K144 controller platform.&lt;/P&gt;&lt;P&gt;We are facing issues receiving and transmitting CAN messages using&amp;nbsp;NXP&amp;nbsp;Support Package on MATLAB for this controller.&lt;/P&gt;&lt;P&gt;While we can Rx CAN message if a dedicated "Message Buffer" is provided for each ID in "FCAN_Receive" block settings, but this is not a ideal solution. The number of "Message Buffer" has a limit of 15. So we could not have dedicated message buffer for each Rx message if we have more than 15 messages.&lt;/P&gt;&lt;P&gt;We have quite a lot of CAN IDs to send and receive on bus and hence would need a mask to receive multiple IDs with same "Message Buffer". We tried using mask but that is not working for us.&lt;/P&gt;&lt;P&gt;We could not receive messages properly, if we put a common "Message Buffer" and some ID mask.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 28 Jan 2026 04:45:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Issue-with-CAN-Communication-using-NXP-Controller-and-MBDT-on/m-p/2301789#M10612</guid>
      <dc:creator>ashutoshsahu</dc:creator>
      <dc:date>2026-01-28T04:45:12Z</dc:date>
    </item>
  </channel>
</rss>