<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 Bulk Pin Configuration using MBDT S32 CT</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Bulk-Pin-Configuration-using-MBDT-S32-CT/m-p/2298525#M10609</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am working with S32K3 using MBDT (Model-Based Design Toolbox) and S32 Configuration Tools v1.8.&lt;BR /&gt;I would like to understand the recommended approach for bulk GPIO / DIO pin configuration.&lt;/P&gt;&lt;P&gt;Current Observation&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;In the Pins Tool, it is not possible to multi-select or bulk-select MCU pins using Ctrl / Shift.&lt;/LI&gt;&lt;LI&gt;Each pin needs to be configured individually through the UI.&lt;/LI&gt;&lt;LI&gt;DIO configuration is derived from the Pins (PORT) configuration, not directly from the DIO driver.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Questions&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is bulk pin configuration (GPIO direction, pull-up/down, initial level) supported in the S32 Configuration Tools v1.8 UI?&lt;/LI&gt;&lt;LI&gt;If UI-based bulk selection is not supported, what is the recommended and supported workaround?&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;Export Pins to CSV and re-import using Data Manager?&lt;/LI&gt;&lt;LI&gt;Import AUTOSAR ECU configuration (ARXML)?&lt;/LI&gt;&lt;/UL&gt;&lt;LI&gt;For MBDT-based projects, is Export Configuration (*.mex) sufficient after updating pin configurations?&lt;/LI&gt;&lt;LI&gt;Is there any plan to support multi-pin selection or bulk editing in future releases?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance or best practices from NXP or experienced users would be appreciated.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Surya S&lt;/P&gt;</description>
    <pubDate>Thu, 22 Jan 2026 17:51:51 GMT</pubDate>
    <dc:creator>suryadevise</dc:creator>
    <dc:date>2026-01-22T17:51:51Z</dc:date>
    <item>
      <title>Bulk Pin Configuration using MBDT S32 CT</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Bulk-Pin-Configuration-using-MBDT-S32-CT/m-p/2298525#M10609</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am working with S32K3 using MBDT (Model-Based Design Toolbox) and S32 Configuration Tools v1.8.&lt;BR /&gt;I would like to understand the recommended approach for bulk GPIO / DIO pin configuration.&lt;/P&gt;&lt;P&gt;Current Observation&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;In the Pins Tool, it is not possible to multi-select or bulk-select MCU pins using Ctrl / Shift.&lt;/LI&gt;&lt;LI&gt;Each pin needs to be configured individually through the UI.&lt;/LI&gt;&lt;LI&gt;DIO configuration is derived from the Pins (PORT) configuration, not directly from the DIO driver.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Questions&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is bulk pin configuration (GPIO direction, pull-up/down, initial level) supported in the S32 Configuration Tools v1.8 UI?&lt;/LI&gt;&lt;LI&gt;If UI-based bulk selection is not supported, what is the recommended and supported workaround?&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;Export Pins to CSV and re-import using Data Manager?&lt;/LI&gt;&lt;LI&gt;Import AUTOSAR ECU configuration (ARXML)?&lt;/LI&gt;&lt;/UL&gt;&lt;LI&gt;For MBDT-based projects, is Export Configuration (*.mex) sufficient after updating pin configurations?&lt;/LI&gt;&lt;LI&gt;Is there any plan to support multi-pin selection or bulk editing in future releases?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Any guidance or best practices from NXP or experienced users would be appreciated.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Surya S&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jan 2026 17:51:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Bulk-Pin-Configuration-using-MBDT-S32-CT/m-p/2298525#M10609</guid>
      <dc:creator>suryadevise</dc:creator>
      <dc:date>2026-01-22T17:51:51Z</dc:date>
    </item>
  </channel>
</rss>