<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: FreeMaster 3.2 not working with S32k344</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-3-2-not-working-with-S32k344/m-p/2298723#M10608</link>
    <description>I want to stick to MBDT 1.5.&lt;BR /&gt;We have performed multiple tests using the FreeMASTER blocks provided with the toolbox, but the results show that FreeMASTER is not working properly.&lt;BR /&gt;Could you please check the model shared in the previous post and make it work for me, or provide a similar model that is compatible with and works correctly with MBDT 1.5?&lt;BR /&gt;Thanks</description>
    <pubDate>Fri, 23 Jan 2026 05:11:36 GMT</pubDate>
    <dc:creator>KaleRushikesh</dc:creator>
    <dc:date>2026-01-23T05:11:36Z</dc:date>
    <item>
      <title>FreeMaster 3.2 not working with S32k344</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-3-2-not-working-with-S32k344/m-p/2295994#M10595</link>
      <description>&lt;P&gt;Hello NXP MBDT Team,&lt;/P&gt;&lt;P&gt;I am working freemaster3.2 on S32k344 and MBDT1.5.&lt;BR /&gt;I am facing a weird issue like, when I am configuring the single CAN0 with single Rx-Tx CAN object, the free master works.&lt;BR /&gt;But on configuring more CAN instances with respective single Rx-Tx object the free master stopped working. i have attached the model for your reference where I am calling the free master APIs, because the same issue was face with free master block also.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jan 2026 12:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-3-2-not-working-with-S32k344/m-p/2295994#M10595</guid>
      <dc:creator>KaleRushikesh</dc:creator>
      <dc:date>2026-01-19T12:21:23Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster 3.2 not working with S32k344</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-3-2-not-working-with-S32k344/m-p/2298219#M10600</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;May I ask why do you custom code for the FreeMASTER? Why don't you use the included blocks for FreeMASTER?&lt;/P&gt;
&lt;P&gt;Moreover, if you don't have any hard limitation, I recommend you to install the latest version for S32K3 Toolbox (v1.8.0).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Sorin Bancila&lt;/P&gt;</description>
      <pubDate>Thu, 22 Jan 2026 10:46:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-3-2-not-working-with-S32k344/m-p/2298219#M10600</guid>
      <dc:creator>SorinIBancila</dc:creator>
      <dc:date>2026-01-22T10:46:47Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster 3.2 not working with S32k344</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-3-2-not-working-with-S32k344/m-p/2298723#M10608</link>
      <description>I want to stick to MBDT 1.5.&lt;BR /&gt;We have performed multiple tests using the FreeMASTER blocks provided with the toolbox, but the results show that FreeMASTER is not working properly.&lt;BR /&gt;Could you please check the model shared in the previous post and make it work for me, or provide a similar model that is compatible with and works correctly with MBDT 1.5?&lt;BR /&gt;Thanks</description>
      <pubDate>Fri, 23 Jan 2026 05:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-3-2-not-working-with-S32k344/m-p/2298723#M10608</guid>
      <dc:creator>KaleRushikesh</dc:creator>
      <dc:date>2026-01-23T05:11:36Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster 3.2 not working with S32k344</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-3-2-not-working-with-S32k344/m-p/2305248#M10619</link>
      <description>Can anyone get the issue.</description>
      <pubDate>Tue, 03 Feb 2026 10:52:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-3-2-not-working-with-S32k344/m-p/2305248#M10619</guid>
      <dc:creator>KaleRushikesh</dc:creator>
      <dc:date>2026-02-03T10:52:22Z</dc:date>
    </item>
  </channel>
</rss>