<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MBDT: S32K144 - No such file or directory in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-S32K144-No-such-file-or-directory/m-p/2204167#M10525</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;Do you know which NXP add-ons are compatible and tested on 2025b ?&lt;/P&gt;&lt;P&gt;1. Try deleting the&amp;nbsp;gpio_s32k144_mbd_rtw&amp;nbsp;folder, together with the slprj folder and try generating code again.&lt;/P&gt;&lt;P&gt;-&amp;gt; No change, still have the errors&lt;/P&gt;&lt;P&gt;2. Try uninstalling and installing the toolbox in a shorter path with no spaces and then try again. You can do that by adjusting first the MATLAB Add-Ons Settings under the Intallation Folder in Settings -&amp;gt; MATLAB -&amp;gt; Add-Ons.&lt;/P&gt;&lt;P&gt;-&amp;gt; i modified the add o path in&amp;nbsp;&lt;SPAN&gt;C:\Users\stefp\AppData\Roaming\MathWorks\MATLAB_Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;still the same error but now the toolchain used is "MinGW64 | gmake (64-bit Windows)" i do not have the option for S32DS GCC anymore&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 13 Nov 2025 06:10:22 GMT</pubDate>
    <dc:creator>StephP</dc:creator>
    <dc:date>2025-11-13T06:10:22Z</dc:date>
    <item>
      <title>MBDT: S32K144 - No such file or directory</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-S32K144-No-such-file-or-directory/m-p/2201772#M10510</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;I just Installed MATLAB 2025b on my computer with all the add-on to work with NXP S32K1XX and i try the "gpio-S32K144" example and i have file error directory or not existing error.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Can you help me please&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Nov 2025 09:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-S32K144-No-such-file-or-directory/m-p/2201772#M10510</guid>
      <dc:creator>StephP</dc:creator>
      <dc:date>2025-11-10T09:56:57Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT: S32K144 - No such file or directory</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-S32K144-No-such-file-or-directory/m-p/2203517#M10520</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256717"&gt;@StephP&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;First of all, i want to mention that the MBDT for S32K1 has been release in 2022 and it has been only tested on the MATLAB &amp;amp; Simulink versions from&amp;nbsp;&lt;SPAN&gt;R2016a to R2022a, which were available on the release date. Unfortunately, there is currently no release planned to address the R2025b. However, I have tried to run the same example on my end on R2025b and it generated the .elf file.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Now, I had a look on your log, and I have some suggestions you might try.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. Try deleting the&amp;nbsp;&lt;CODE class="bp-text-code txt"&gt;gpio_s32k144_mbd_rtw&lt;/CODE&gt;&amp;nbsp;folder, together with the slprj folder and try generating code again.&lt;/P&gt;
&lt;P&gt;2. Try uninstalling and installing the toolbox in a shorter path with no spaces and then try again. You can do that by adjusting first the MATLAB Add-Ons Settings under the Intallation Folder in Settings -&amp;gt; MATLAB -&amp;gt; Add-Ons.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="mariuslucianand_0-1762942149318.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/365219iE3E09292C66EA223/image-size/medium?v=v2&amp;amp;px=400" role="button" title="mariuslucianand_0-1762942149318.png" alt="mariuslucianand_0-1762942149318.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope this helps,&lt;/P&gt;
&lt;P&gt;Marius&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Nov 2025 10:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-S32K144-No-such-file-or-directory/m-p/2203517#M10520</guid>
      <dc:creator>mariuslucianand</dc:creator>
      <dc:date>2025-11-12T10:09:59Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT: S32K144 - No such file or directory</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-S32K144-No-such-file-or-directory/m-p/2204167#M10525</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/72088"&gt;@mariuslucianand&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;Do you know which NXP add-ons are compatible and tested on 2025b ?&lt;/P&gt;&lt;P&gt;1. Try deleting the&amp;nbsp;gpio_s32k144_mbd_rtw&amp;nbsp;folder, together with the slprj folder and try generating code again.&lt;/P&gt;&lt;P&gt;-&amp;gt; No change, still have the errors&lt;/P&gt;&lt;P&gt;2. Try uninstalling and installing the toolbox in a shorter path with no spaces and then try again. You can do that by adjusting first the MATLAB Add-Ons Settings under the Intallation Folder in Settings -&amp;gt; MATLAB -&amp;gt; Add-Ons.&lt;/P&gt;&lt;P&gt;-&amp;gt; i modified the add o path in&amp;nbsp;&lt;SPAN&gt;C:\Users\stefp\AppData\Roaming\MathWorks\MATLAB_Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;still the same error but now the toolchain used is "MinGW64 | gmake (64-bit Windows)" i do not have the option for S32DS GCC anymore&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Nov 2025 06:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-S32K144-No-such-file-or-directory/m-p/2204167#M10525</guid>
      <dc:creator>StephP</dc:creator>
      <dc:date>2025-11-13T06:10:22Z</dc:date>
    </item>
  </channel>
</rss>