<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックCan't recognize OpenSDA drive in Simulink but in Device Manager</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Can-t-recognize-OpenSDA-drive-in-Simulink-but-in-Device-Manager/m-p/2160715#M10414</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was trying to use MBDT on S32K144EVB. I was able to see OpenSDA port in Device Manager, file explorer as a USB thumb drive as D. But I Simulink couldn't recognize the drive.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="weizhongsmp_0-1756474010674.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354820i582FE6F38650A6EE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="weizhongsmp_0-1756474010674.png" alt="weizhongsmp_0-1756474010674.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If I use Custom with Drive D:, then Simulink would stuck in generating code after build. It doesn't seem to be able to download to the board. And the board seems to be in a loop as well trying to boot up, with red LED quickly flashes and green LED flashes 5 times.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I saw similar posts from other members and I couldn't fix the issue. I think it might have to do with this unrecognized OpenSDA drive.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 29 Aug 2025 13:29:56 GMT</pubDate>
    <dc:creator>WWsmp</dc:creator>
    <dc:date>2025-08-29T13:29:56Z</dc:date>
    <item>
      <title>Can't recognize OpenSDA drive in Simulink but in Device Manager</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Can-t-recognize-OpenSDA-drive-in-Simulink-but-in-Device-Manager/m-p/2160715#M10414</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was trying to use MBDT on S32K144EVB. I was able to see OpenSDA port in Device Manager, file explorer as a USB thumb drive as D. But I Simulink couldn't recognize the drive.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="weizhongsmp_0-1756474010674.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354820i582FE6F38650A6EE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="weizhongsmp_0-1756474010674.png" alt="weizhongsmp_0-1756474010674.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If I use Custom with Drive D:, then Simulink would stuck in generating code after build. It doesn't seem to be able to download to the board. And the board seems to be in a loop as well trying to boot up, with red LED quickly flashes and green LED flashes 5 times.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I saw similar posts from other members and I couldn't fix the issue. I think it might have to do with this unrecognized OpenSDA drive.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Aug 2025 13:29:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Can-t-recognize-OpenSDA-drive-in-Simulink-but-in-Device-Manager/m-p/2160715#M10414</guid>
      <dc:creator>WWsmp</dc:creator>
      <dc:date>2025-08-29T13:29:56Z</dc:date>
    </item>
  </channel>
</rss>