<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 Does MM912_637 support Model-Based Tool Box?</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Does-MM912-637-support-Model-Based-Tool-Box/m-p/2160707#M10413</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the battery sensor MM912_637 which is said to be part of S12 family. And in MBDT supported devices, there are two S12 chips that are supported.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just wonder if this MM912_637 supports MBDT, if so which library should I use.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Weizhong&lt;/P&gt;</description>
    <pubDate>Fri, 29 Aug 2025 13:23:02 GMT</pubDate>
    <dc:creator>WWsmp</dc:creator>
    <dc:date>2025-08-29T13:23:02Z</dc:date>
    <item>
      <title>Does MM912_637 support Model-Based Tool Box?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Does-MM912-637-support-Model-Based-Tool-Box/m-p/2160707#M10413</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have the battery sensor MM912_637 which is said to be part of S12 family. And in MBDT supported devices, there are two S12 chips that are supported.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just wonder if this MM912_637 supports MBDT, if so which library should I use.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Weizhong&lt;/P&gt;</description>
      <pubDate>Fri, 29 Aug 2025 13:23:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Does-MM912-637-support-Model-Based-Tool-Box/m-p/2160707#M10413</guid>
      <dc:creator>WWsmp</dc:creator>
      <dc:date>2025-08-29T13:23:02Z</dc:date>
    </item>
  </channel>
</rss>