<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic When will MBDT support RTD 6.0.0 and S32DS 3.6? in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/When-will-MBDT-support-RTD-6-0-0-and-S32DS-3-6/m-p/2153158#M10395</link>
    <description>&lt;P&gt;I need to use S32K3 TCP/IP Stack 3.0.0, which is based on RTD 6.0.0 and S32DS 3.6.&lt;BR /&gt;Currently, the latest MBDT version is 1.6.0, based on RTD 5.0.0 and S32DS 3.5.&lt;BR /&gt;May I ask if there are any plans for MBDT to support RTD 6.0.0 and S32DS 3.6, so that I can call TCP/IP 3.0.0 in Custom Code?&lt;/P&gt;&lt;P&gt;Thank you for taking care of this matter.&lt;/P&gt;</description>
    <pubDate>Mon, 18 Aug 2025 01:27:44 GMT</pubDate>
    <dc:creator>pro778tw</dc:creator>
    <dc:date>2025-08-18T01:27:44Z</dc:date>
    <item>
      <title>When will MBDT support RTD 6.0.0 and S32DS 3.6?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/When-will-MBDT-support-RTD-6-0-0-and-S32DS-3-6/m-p/2153158#M10395</link>
      <description>&lt;P&gt;I need to use S32K3 TCP/IP Stack 3.0.0, which is based on RTD 6.0.0 and S32DS 3.6.&lt;BR /&gt;Currently, the latest MBDT version is 1.6.0, based on RTD 5.0.0 and S32DS 3.5.&lt;BR /&gt;May I ask if there are any plans for MBDT to support RTD 6.0.0 and S32DS 3.6, so that I can call TCP/IP 3.0.0 in Custom Code?&lt;/P&gt;&lt;P&gt;Thank you for taking care of this matter.&lt;/P&gt;</description>
      <pubDate>Mon, 18 Aug 2025 01:27:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/When-will-MBDT-support-RTD-6-0-0-and-S32DS-3-6/m-p/2153158#M10395</guid>
      <dc:creator>pro778tw</dc:creator>
      <dc:date>2025-08-18T01:27:44Z</dc:date>
    </item>
    <item>
      <title>Re: When will MBDT support RTD 6.0.0 and S32DS 3.6?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/When-will-MBDT-support-RTD-6-0-0-and-S32DS-3-6/m-p/2154345#M10399</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253848"&gt;@pro778tw&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thank you for your interest into Model-Based Design Toolbox for S32K3.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;STRONG&gt;RTD 6.0.0&lt;/STRONG&gt; and &lt;STRONG&gt;S32DS 3.6&lt;/STRONG&gt; support will be added in the next toolbox version (&lt;STRONG&gt;MBDT S32K3 version 1.7.0&lt;/STRONG&gt;), which will be released at the end of this quarter.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Dragos&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Aug 2025 10:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/When-will-MBDT-support-RTD-6-0-0-and-S32DS-3-6/m-p/2154345#M10399</guid>
      <dc:creator>dragostoma</dc:creator>
      <dc:date>2025-08-19T10:28:45Z</dc:date>
    </item>
  </channel>
</rss>