<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Implement Fee using MBDT1.5 or custom code in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Implement-Fee-using-MBDT1-5-or-custom-code/m-p/2148972#M10385</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253372"&gt;@KaleRushikesh&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please&amp;nbsp;review the related thread for more details:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/integrating-FEE-in-Simulink/m-p/2148969/highlight/true#M10384" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/integrating-FEE-in-Simulink/m-p/2148969/highlight/true#M10384&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Dragos&lt;/P&gt;</description>
    <pubDate>Fri, 08 Aug 2025 07:27:15 GMT</pubDate>
    <dc:creator>dragostoma</dc:creator>
    <dc:date>2025-08-08T07:27:15Z</dc:date>
    <item>
      <title>Implement Fee using MBDT1.5 or custom code</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Implement-Fee-using-MBDT1-5-or-custom-code/m-p/2145104#M10372</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to implement FEE in Simulink, but MBDT 1.5 does not have a library block for FEE.&lt;BR /&gt;So, I referred to the S32DS FEE example, which works in Design Studio. I don’t want to switch toolboxes, but I still want to use FEE in Simulink.&lt;/P&gt;&lt;P&gt;While working on this, I observed that:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;In Simulink, to configure FEE we also need to configure &lt;STRONG&gt;FEE, Mem_43_IFLS, and MemAcc&lt;/STRONG&gt;.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;In S32DS, we only need to configure &lt;STRONG&gt;FEE and FLS&lt;/STRONG&gt;.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Because of this difference, some .h files that are generated by the configuration tool in S32Ds are not generated in case of the configuration done in Simulink setup.&lt;/P&gt;&lt;P&gt;This makes me confused about &lt;STRONG&gt;which APIs I should call from a Simulink MATLAB Function using coder.ceval()&lt;/STRONG&gt;.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Aug 2025 10:15:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Implement-Fee-using-MBDT1-5-or-custom-code/m-p/2145104#M10372</guid>
      <dc:creator>KaleRushikesh</dc:creator>
      <dc:date>2025-08-01T10:15:38Z</dc:date>
    </item>
    <item>
      <title>Re: Implement Fee using MBDT1.5 or custom code</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Implement-Fee-using-MBDT1-5-or-custom-code/m-p/2148972#M10385</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253372"&gt;@KaleRushikesh&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please&amp;nbsp;review the related thread for more details:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/integrating-FEE-in-Simulink/m-p/2148969/highlight/true#M10384" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/integrating-FEE-in-Simulink/m-p/2148969/highlight/true#M10384&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Dragos&lt;/P&gt;</description>
      <pubDate>Fri, 08 Aug 2025 07:27:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Implement-Fee-using-MBDT1-5-or-custom-code/m-p/2148972#M10385</guid>
      <dc:creator>dragostoma</dc:creator>
      <dc:date>2025-08-08T07:27:15Z</dc:date>
    </item>
  </channel>
</rss>