<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: s32k3xx_dio_ebt example on S32K396 BMS EVB</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32k3xx-dio-ebt-example-on-S32K396-BMS-EVB/m-p/2131377#M10338</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The s32k3xx_dio_ebt example on the S32K396 BMS EVB, change the DIO pins to match your board:&lt;/P&gt;&lt;P&gt;Use PTD4, PTD5, and PTH7 for LEDs D34, D33, and D35.&lt;/P&gt;&lt;P&gt;In Simulink, open the DIO block and set these pins.&lt;/P&gt;&lt;P&gt;In the S32 Configuration Tool, route these pins as digital outputs.&lt;/P&gt;&lt;P&gt;Set the board configuration to XS32K396-BGA-DC1.&amp;nbsp;&lt;A href="https://www.peryourhealth.doctor" target="_self"&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FFFFFF"&gt;PerYourHealth&lt;/FONT&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Build and flash the code. Ensure 12 V is supplied and jumpers (J4, J6, J7) are set correctly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regard,&lt;/P&gt;&lt;P&gt;Angela&lt;/P&gt;</description>
    <pubDate>Thu, 10 Jul 2025 04:35:35 GMT</pubDate>
    <dc:creator>angela852black</dc:creator>
    <dc:date>2025-07-10T04:35:35Z</dc:date>
    <item>
      <title>s32k3xx_dio_ebt example on S32K396 BMS EVB</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32k3xx-dio-ebt-example-on-S32K396-BMS-EVB/m-p/2123654#M10316</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using NXP MBDT toolbox in matlab for configuring S32K396 BMS EVB and I checked with Dio example to flash LED. I checked s32k3xx_dio_ebt example on S32K396 BMS EVB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am able to download the code on EVB, but not able to see output. This is because of pin configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This example uses pins of s32k396 bga dc board, I think.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using s32k396 bms evb so which pins I need to select for this example? and how? Please help with step-by-step procedure&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jun 2025 06:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32k3xx-dio-ebt-example-on-S32K396-BMS-EVB/m-p/2123654#M10316</guid>
      <dc:creator>bhushan7051</dc:creator>
      <dc:date>2025-06-26T06:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3xx_dio_ebt example on S32K396 BMS EVB</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32k3xx-dio-ebt-example-on-S32K396-BMS-EVB/m-p/2125352#M10319</link>
      <description>Can I get any help on above issue ?</description>
      <pubDate>Mon, 30 Jun 2025 06:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32k3xx-dio-ebt-example-on-S32K396-BMS-EVB/m-p/2125352#M10319</guid>
      <dc:creator>bhushan7051</dc:creator>
      <dc:date>2025-06-30T06:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3xx_dio_ebt example on S32K396 BMS EVB</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32k3xx-dio-ebt-example-on-S32K396-BMS-EVB/m-p/2130813#M10337</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I help for this&amp;nbsp;&lt;/P&gt;&lt;P&gt;Open your Simulink model with the s32k3xx_dio_ebt example.&lt;/P&gt;&lt;P&gt;Double‑click the Dio block and click Configure… to launch the S32 Configuration Tool (S32CT) or EB Tresos depending on your setup&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Identify the EVB's LED GPIOs&lt;BR /&gt;The BMS EVB is significantly different:&lt;/P&gt;&lt;P&gt;It’s not the same as the BGA‑DC1 board (PTH7, PTD4, PTD5 in DC1).&lt;/P&gt;&lt;P&gt;You’ll need to refer to the S32K396BMS‑EVB schematics/user manual to find exactly which pins are physically wired to LEDs on that board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Assign the Correct PortPins in Configuration Tool&lt;BR /&gt;Once you have identified the LED GPIO pins (e.g., PTxY notation):&lt;/P&gt;&lt;P&gt;In S32CT:&lt;/P&gt;&lt;P&gt;Go to the Pins/routing section.&lt;/P&gt;&lt;P&gt;Add each LED, configure the correct PortPin, MSCR, and SiUL2 details to match the EVB hardware.&lt;/P&gt;&lt;P&gt;In EB Tresos (if used):&lt;/P&gt;&lt;P&gt;Do the same pin assignments within the EB configuration XML.&lt;/P&gt;&lt;P&gt;Update the Dio Block in Simulink&lt;BR /&gt;In your Simulink model’s Dio block parameters:&lt;/P&gt;&lt;P&gt;Replace the default pin/channel (which corresponded to the DC1 or Q289 board) with your EVB pins.&lt;/P&gt;&lt;P&gt;For example, if LED1 is on PTC3 (GPIO78), set channel = 78.&lt;/P&gt;&lt;P&gt;Click Apply and OK.&lt;/P&gt;&lt;P&gt;Rebuild, Flash, and Test&lt;BR /&gt;Press Download to flash the code.&lt;/P&gt;&lt;P&gt;The board is powered (12 V external) and jumpers are properly set&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regard,&lt;/P&gt;&lt;P&gt;Angela&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 09:41:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32k3xx-dio-ebt-example-on-S32K396-BMS-EVB/m-p/2130813#M10337</guid>
      <dc:creator>angela852black</dc:creator>
      <dc:date>2025-07-09T09:41:00Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3xx_dio_ebt example on S32K396 BMS EVB</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32k3xx-dio-ebt-example-on-S32K396-BMS-EVB/m-p/2131377#M10338</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The s32k3xx_dio_ebt example on the S32K396 BMS EVB, change the DIO pins to match your board:&lt;/P&gt;&lt;P&gt;Use PTD4, PTD5, and PTH7 for LEDs D34, D33, and D35.&lt;/P&gt;&lt;P&gt;In Simulink, open the DIO block and set these pins.&lt;/P&gt;&lt;P&gt;In the S32 Configuration Tool, route these pins as digital outputs.&lt;/P&gt;&lt;P&gt;Set the board configuration to XS32K396-BGA-DC1.&amp;nbsp;&lt;A href="https://www.peryourhealth.doctor" target="_self"&gt;&lt;FONT size="1 2 3 4 5 6 7" color="#FFFFFF"&gt;PerYourHealth&lt;/FONT&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Build and flash the code. Ensure 12 V is supplied and jumpers (J4, J6, J7) are set correctly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regard,&lt;/P&gt;&lt;P&gt;Angela&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jul 2025 04:35:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/s32k3xx-dio-ebt-example-on-S32K396-BMS-EVB/m-p/2131377#M10338</guid>
      <dc:creator>angela852black</dc:creator>
      <dc:date>2025-07-10T04:35:35Z</dc:date>
    </item>
  </channel>
</rss>