<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC DMA Example doesn't work with my S32CT Configuration in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/ADC-DMA-Example-doesn-t-work-with-my-S32CT-Configuration/m-p/2124851#M10317</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i'm trying the ADC-DMA Example on&amp;nbsp;S32K3X8EVB-Q289.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried to configure the ADC module by myself based on the S32CT configuration given with the example ( all seems the same on S32CT).&lt;/P&gt;&lt;P&gt;When i download my application on the board the adc callback it's executed correctly because i've put a toggle-led block inside it and i could see the led blinking.&lt;/P&gt;&lt;P&gt;The problem is that it does not do the conversion....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've also tried to import the example's&lt;SPAN&gt;&amp;nbsp;configuration of the ADC and RM modules in my configuration file (.mex)... Surprisingly it converts only one time after the initialization but not continuously...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Confronting the 2 .mex&amp;nbsp;&lt;SPAN&gt;file i could see that the differences seems to be some parts of the ADC module that are written in different places in the .mex files .... i don't know why....&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'd need some help to understand and fix this thing as i don't want to fall on it again in the future... I attach my model with both the files, the one created by me and the other with the mudels imported from the example...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Simon&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 27 Jun 2025 14:50:21 GMT</pubDate>
    <dc:creator>simon98</dc:creator>
    <dc:date>2025-06-27T14:50:21Z</dc:date>
    <item>
      <title>ADC DMA Example doesn't work with my S32CT Configuration</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/ADC-DMA-Example-doesn-t-work-with-my-S32CT-Configuration/m-p/2124851#M10317</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i'm trying the ADC-DMA Example on&amp;nbsp;S32K3X8EVB-Q289.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried to configure the ADC module by myself based on the S32CT configuration given with the example ( all seems the same on S32CT).&lt;/P&gt;&lt;P&gt;When i download my application on the board the adc callback it's executed correctly because i've put a toggle-led block inside it and i could see the led blinking.&lt;/P&gt;&lt;P&gt;The problem is that it does not do the conversion....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've also tried to import the example's&lt;SPAN&gt;&amp;nbsp;configuration of the ADC and RM modules in my configuration file (.mex)... Surprisingly it converts only one time after the initialization but not continuously...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Confronting the 2 .mex&amp;nbsp;&lt;SPAN&gt;file i could see that the differences seems to be some parts of the ADC module that are written in different places in the .mex files .... i don't know why....&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'd need some help to understand and fix this thing as i don't want to fall on it again in the future... I attach my model with both the files, the one created by me and the other with the mudels imported from the example...&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Simon&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jun 2025 14:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/ADC-DMA-Example-doesn-t-work-with-my-S32CT-Configuration/m-p/2124851#M10317</guid>
      <dc:creator>simon98</dc:creator>
      <dc:date>2025-06-27T14:50:21Z</dc:date>
    </item>
    <item>
      <title>Re: ADC DMA Example doesn't work with my S32CT Configuration</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/ADC-DMA-Example-doesn-t-work-with-my-S32CT-Configuration/m-p/2125675#M10320</link>
      <description>&lt;P&gt;I've found out that using the configuration imported form the example .mex, if i start the communication with my FreeMASTER project it works correctly showing me the adc output value changing while moving the potentiometer on the board...&lt;/P&gt;&lt;P&gt;I don't understand this behavior... could someone help?&lt;/P&gt;&lt;P&gt;I attach my FreeMASATER project&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jun 2025 13:41:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/ADC-DMA-Example-doesn-t-work-with-my-S32CT-Configuration/m-p/2125675#M10320</guid>
      <dc:creator>simon98</dc:creator>
      <dc:date>2025-06-30T13:41:20Z</dc:date>
    </item>
    <item>
      <title>Re: ADC DMA Example doesn't work with my S32CT Configuration</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/ADC-DMA-Example-doesn-t-work-with-my-S32CT-Configuration/m-p/2130783#M10336</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;i have questions on all three points you've mentioned:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;1) the conversion trigger source is SW and it's been done every 10 ms by Adc_StartGroupConversion.&lt;/P&gt;&lt;P&gt;2)"&lt;EM&gt;&lt;STRONG&gt;DMA configuration&lt;/STRONG&gt;&amp;nbsp;— it might be set to stop after one transfer unless it’s explicitly looped or retriggered.&lt;/EM&gt;" where i'm a able to see if DMA configuration is doing that? cause i screened all madules of the DMA example and confronted with mine .mex and there's literally no difference...&lt;/P&gt;&lt;P&gt;3)what do you mean with &lt;STRONG&gt;ADC command&amp;nbsp; list&lt;/STRONG&gt;?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is not clear yet how is that the .mex configured by meworks differently from a .mex with imported configuration from the DMA example...&lt;/P&gt;&lt;P&gt;Could you please check the project attached if presents the same behavior with both .mex?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 09:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/ADC-DMA-Example-doesn-t-work-with-my-S32CT-Configuration/m-p/2130783#M10336</guid>
      <dc:creator>simon98</dc:creator>
      <dc:date>2025-07-09T09:06:28Z</dc:date>
    </item>
  </channel>
</rss>