<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: DIO Write Channel not working</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DIO-Write-Channel-not-working/m-p/2117555#M10297</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;do you have Port component configured as well as article showed?&lt;BR /&gt;Further I can recommend to check respective SIUL2 MSCR and GPDO setting in the debugger.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jun 2025 08:04:43 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2025-06-17T08:04:43Z</dc:date>
    <item>
      <title>DIO Write Channel not working</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DIO-Write-Channel-not-working/m-p/2117225#M10294</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I have an NXP S32K312 EVB and I am trying to set a pin high all the time. For this, I have followed the steps mentioned in this article -&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Interacting-with-Digital-Inputs-Outputs-on-MR-CANHUBK344/ta-p/1746789" target="_blank"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Interacting-with-Digital-Inputs-Outputs-on-MR-CANHUBK344/ta-p/1746789&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I want to use PTA 28 and this is how it is configured in NXPS32CT.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="schitta_0-1750107412629.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/343169i74D83CAC194A4104/image-size/medium?v=v2&amp;amp;px=400" role="button" title="schitta_0-1750107412629.png" alt="schitta_0-1750107412629.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Here's the view of Pin configuration "Dio_Pins_MBDT" for PTA28&lt;BR /&gt;&lt;BR /&gt;Also, tried setting the Initial value of Pin to High as shown in snippet&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="schitta_1-1750107513939.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/343170iCA2B6FC7D142EE0B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="schitta_1-1750107513939.png" alt="schitta_1-1750107513939.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the simulink model, I'm simply using a data store memory block to write a value of 1&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="schitta_2-1750107611403.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/343171iF745CBD8F4C702AB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="schitta_2-1750107611403.png" alt="schitta_2-1750107611403.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I do not see the pin actually going high with this setup and config.&amp;nbsp;When I measure voltage, it is about 0.13 V and also tried to probe the same pin but it always stays low. Please let me know what I could be missing. Thanks!!&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jun 2025 21:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DIO-Write-Channel-not-working/m-p/2117225#M10294</guid>
      <dc:creator>beginner100</dc:creator>
      <dc:date>2025-06-16T21:01:45Z</dc:date>
    </item>
    <item>
      <title>Re: DIO Write Channel not working</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DIO-Write-Channel-not-working/m-p/2117555#M10297</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;do you have Port component configured as well as article showed?&lt;BR /&gt;Further I can recommend to check respective SIUL2 MSCR and GPDO setting in the debugger.&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 08:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/DIO-Write-Channel-not-working/m-p/2117555#M10297</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-06-17T08:04:43Z</dc:date>
    </item>
  </channel>
</rss>