<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: RTC alarm set s32k144 MATLAB simulink MBDT example</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RTC-alarm-set-s32k144-MATLAB-simulink-MBDT-example/m-p/2110390#M10276</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you can access low-level registers or custom driver code (via S32 SDK or S32 Design Studio), then:&lt;/P&gt;&lt;P&gt;Read current RTC time from RTC_TSR.&lt;/P&gt;&lt;P&gt;Set RTC_TAR = RTC_TSR + desired_offset_in_seconds.&lt;/P&gt;&lt;P&gt;Ensure RTC_IER has the alarm interrupt enabled.&lt;/P&gt;&lt;P&gt;Make sure your RTC module clock is properly set.&lt;/P&gt;&lt;P&gt;Check boundary conditions if RTC_TAR overflows a minute or hour — handle it gracefully.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regard,&lt;/P&gt;&lt;P&gt;Helen&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 04 Jun 2025 11:40:20 GMT</pubDate>
    <dc:creator>helen628young</dc:creator>
    <dc:date>2025-06-04T11:40:20Z</dc:date>
    <item>
      <title>RTC alarm set s32k144 MATLAB simulink MBDT example</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RTC-alarm-set-s32k144-MATLAB-simulink-MBDT-example/m-p/2110357#M10275</link>
      <description>&lt;P&gt;I am using MATLAB Simulink example for RTC Alarm for S32K144 , The RTC Get time and RTC Alarm set is used int it to set RTC alarm ISR when ever I want to set ISR more than 25 sec from RTC get time but the ISR is not triggered , The ISR is triggered for all values from 1-25 sec from the RTC get time but not more than the 25sec. What is the cause of this , explain the process behind it and how to over this and implement to kick RTC alarm after for higher time interval.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 10:35:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RTC-alarm-set-s32k144-MATLAB-simulink-MBDT-example/m-p/2110357#M10275</guid>
      <dc:creator>Haris_raghav_G</dc:creator>
      <dc:date>2025-06-04T10:35:47Z</dc:date>
    </item>
    <item>
      <title>Re: RTC alarm set s32k144 MATLAB simulink MBDT example</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RTC-alarm-set-s32k144-MATLAB-simulink-MBDT-example/m-p/2110390#M10276</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you can access low-level registers or custom driver code (via S32 SDK or S32 Design Studio), then:&lt;/P&gt;&lt;P&gt;Read current RTC time from RTC_TSR.&lt;/P&gt;&lt;P&gt;Set RTC_TAR = RTC_TSR + desired_offset_in_seconds.&lt;/P&gt;&lt;P&gt;Ensure RTC_IER has the alarm interrupt enabled.&lt;/P&gt;&lt;P&gt;Make sure your RTC module clock is properly set.&lt;/P&gt;&lt;P&gt;Check boundary conditions if RTC_TAR overflows a minute or hour — handle it gracefully.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regard,&lt;/P&gt;&lt;P&gt;Helen&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 11:40:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/RTC-alarm-set-s32k144-MATLAB-simulink-MBDT-example/m-p/2110390#M10276</guid>
      <dc:creator>helen628young</dc:creator>
      <dc:date>2025-06-04T11:40:20Z</dc:date>
    </item>
  </channel>
</rss>