<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRequest for Validation, Peripheral Clock Setup via s32k_clock_init.c in Simulink Projects (S32K116)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Request-for-Validation-Peripheral-Clock-Setup-via-s32k-clock/m-p/2099160#M10253</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are supporting a customer working with the S32K116 and the NXP MBDToolbox v4.3.0 for MATLAB/Simulink.&lt;/P&gt;&lt;P&gt;The customer experienced issues when switching from external to internal clocks, particularly with peripheral modules like ADC, LPIT, and FTM not being initialized correctly unless manually configured. To provide a more robust and maintainable approach, we proposed centralizing all peripheral clock settings using the clock_manager_user_config_t structure inside a custom s32k_clock_init.c file.&lt;/P&gt;&lt;P&gt;We have attached both the original file provided by the customer and a cleaned-up version we prepared, based on the recommended ClockManager structure and peripheral configuration approach.&lt;/P&gt;&lt;P&gt;We would appreciate your feedback on the following points:&lt;/P&gt;&lt;P&gt;1. Does this centralized configuration approach align with best practices for projects using the MBDToolbox?&lt;BR /&gt;2. Could there be any conflicts or unintended behavior when peripheral blocks in the Simulink model also generate their own initialization code?&lt;BR /&gt;3. Are there any known issues or constraints when using manual ClockManager-based configuration in parallel with Simulink-generated code?&lt;/P&gt;&lt;P&gt;If this falls outside the scope of your team, we would appreciate it if you could help redirect this to the appropriate contact within NXP.&lt;/P&gt;&lt;P&gt;Thank you in advance for your time and support.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Fri, 16 May 2025 19:10:56 GMT</pubDate>
    <dc:creator>VictorPastrana</dc:creator>
    <dc:date>2025-05-16T19:10:56Z</dc:date>
    <item>
      <title>Request for Validation, Peripheral Clock Setup via s32k_clock_init.c in Simulink Projects (S32K116)</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Request-for-Validation-Peripheral-Clock-Setup-via-s32k-clock/m-p/2099160#M10253</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are supporting a customer working with the S32K116 and the NXP MBDToolbox v4.3.0 for MATLAB/Simulink.&lt;/P&gt;&lt;P&gt;The customer experienced issues when switching from external to internal clocks, particularly with peripheral modules like ADC, LPIT, and FTM not being initialized correctly unless manually configured. To provide a more robust and maintainable approach, we proposed centralizing all peripheral clock settings using the clock_manager_user_config_t structure inside a custom s32k_clock_init.c file.&lt;/P&gt;&lt;P&gt;We have attached both the original file provided by the customer and a cleaned-up version we prepared, based on the recommended ClockManager structure and peripheral configuration approach.&lt;/P&gt;&lt;P&gt;We would appreciate your feedback on the following points:&lt;/P&gt;&lt;P&gt;1. Does this centralized configuration approach align with best practices for projects using the MBDToolbox?&lt;BR /&gt;2. Could there be any conflicts or unintended behavior when peripheral blocks in the Simulink model also generate their own initialization code?&lt;BR /&gt;3. Are there any known issues or constraints when using manual ClockManager-based configuration in parallel with Simulink-generated code?&lt;/P&gt;&lt;P&gt;If this falls outside the scope of your team, we would appreciate it if you could help redirect this to the appropriate contact within NXP.&lt;/P&gt;&lt;P&gt;Thank you in advance for your time and support.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Fri, 16 May 2025 19:10:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Request-for-Validation-Peripheral-Clock-Setup-via-s32k-clock/m-p/2099160#M10253</guid>
      <dc:creator>VictorPastrana</dc:creator>
      <dc:date>2025-05-16T19:10:56Z</dc:date>
    </item>
    <item>
      <title>Re: Request for Validation, Peripheral Clock Setup via s32k_clock_init.c in Simulink Projects (S32K1</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Request-for-Validation-Peripheral-Clock-Setup-via-s32k-clock/m-p/2105447#M10263</link>
      <description>Any help?</description>
      <pubDate>Tue, 27 May 2025 17:12:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Request-for-Validation-Peripheral-Clock-Setup-via-s32k-clock/m-p/2105447#M10263</guid>
      <dc:creator>VictorPastrana</dc:creator>
      <dc:date>2025-05-27T17:12:04Z</dc:date>
    </item>
  </channel>
</rss>