<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックMatlab 23b and S32K3x4EVL-T172</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Matlab-23b-and-S32K3x4EVL-T172/m-p/2089984#M10242</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I used Matlab/Simulink (version 23a) to build a simple model to make the RGB LEDs flash on a eval board (S32K3x4EVB-T172). This also works. Now I have updated Matlab to version 23b and have also partially renewed or updated the toolboxes. The model is still compiled correctly and flashed on the board but unfortunately the LED does not flash.&lt;BR /&gt;Even a simple FreeMaster example no longer runs with version 23b.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Are there any problems with the BSP?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Apr 2025 07:49:00 GMT</pubDate>
    <dc:creator>AlexG124</dc:creator>
    <dc:date>2025-04-30T07:49:00Z</dc:date>
    <item>
      <title>Matlab 23b and S32K3x4EVL-T172</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Matlab-23b-and-S32K3x4EVL-T172/m-p/2089984#M10242</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I used Matlab/Simulink (version 23a) to build a simple model to make the RGB LEDs flash on a eval board (S32K3x4EVB-T172). This also works. Now I have updated Matlab to version 23b and have also partially renewed or updated the toolboxes. The model is still compiled correctly and flashed on the board but unfortunately the LED does not flash.&lt;BR /&gt;Even a simple FreeMaster example no longer runs with version 23b.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Are there any problems with the BSP?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Apr 2025 07:49:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Matlab-23b-and-S32K3x4EVL-T172/m-p/2089984#M10242</guid>
      <dc:creator>AlexG124</dc:creator>
      <dc:date>2025-04-30T07:49:00Z</dc:date>
    </item>
  </channel>
</rss>