<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 MBDT for RDBESS772BJBEVB evaluation board and MC33772C IC</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-for-RDBESS772BJBEVB-evaluation-board-and-MC33772C-IC/m-p/2079998#M10219</link>
    <description>&lt;P&gt;We are currently using the NXP 1500V BMS evaluation board (RD-BESS1500BUN), along with NXP's model-based design tools (MBDT) in MATLAB/Simulink to develop our BMS software.&amp;nbsp;Since configuring BMS IC specifications using MBDT is quite complex, we would greatly appreciate your guidance or the provision of a more complete example model that includes the secondary features.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;As with the RD-BESS1500BUN, the MBDT example for the RDBESS772BJBEVB only activates basic features.&lt;BR /&gt;Specifically:&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;Several high-voltage measurement ports (four positive and two bipolar inputs) are not accessible in the MBDT model.&lt;/LI&gt;&lt;LI&gt;The board also supports precharge resistor temperature monitoring using an external sensor, but MBDT blocks for this feature are missing.&lt;/LI&gt;&lt;/UL&gt;&lt;/OL&gt;&lt;P&gt;Could you please provide guidance or updated MBDT examples that include these features? Thank you sincerely for your continued support and assistance.Regards&lt;BR /&gt;Rasoul&lt;/P&gt;</description>
    <pubDate>Mon, 14 Apr 2025 13:29:13 GMT</pubDate>
    <dc:creator>Rasoul</dc:creator>
    <dc:date>2025-04-14T13:29:13Z</dc:date>
    <item>
      <title>MBDT for RDBESS772BJBEVB evaluation board and MC33772C IC</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-for-RDBESS772BJBEVB-evaluation-board-and-MC33772C-IC/m-p/2079998#M10219</link>
      <description>&lt;P&gt;We are currently using the NXP 1500V BMS evaluation board (RD-BESS1500BUN), along with NXP's model-based design tools (MBDT) in MATLAB/Simulink to develop our BMS software.&amp;nbsp;Since configuring BMS IC specifications using MBDT is quite complex, we would greatly appreciate your guidance or the provision of a more complete example model that includes the secondary features.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;As with the RD-BESS1500BUN, the MBDT example for the RDBESS772BJBEVB only activates basic features.&lt;BR /&gt;Specifically:&lt;/LI&gt;&lt;UL&gt;&lt;LI&gt;Several high-voltage measurement ports (four positive and two bipolar inputs) are not accessible in the MBDT model.&lt;/LI&gt;&lt;LI&gt;The board also supports precharge resistor temperature monitoring using an external sensor, but MBDT blocks for this feature are missing.&lt;/LI&gt;&lt;/UL&gt;&lt;/OL&gt;&lt;P&gt;Could you please provide guidance or updated MBDT examples that include these features? Thank you sincerely for your continued support and assistance.Regards&lt;BR /&gt;Rasoul&lt;/P&gt;</description>
      <pubDate>Mon, 14 Apr 2025 13:29:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT-for-RDBESS772BJBEVB-evaluation-board-and-MC33772C-IC/m-p/2079998#M10219</guid>
      <dc:creator>Rasoul</dc:creator>
      <dc:date>2025-04-14T13:29:13Z</dc:date>
    </item>
  </channel>
</rss>