<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Change CAN Baud Rate in S32K3 Board in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Change-CAN-Baud-Rate-in-S32K3-Board/m-p/2075941#M10203</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi Community,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm new to MBDT and working with the S32K344. I'm setting up a basic CAN communication between the S32K344 and CAN Analyzer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The default settings are for 1 Mbps, but I need to run the CAN at 500 kbps. Which parameters should I adjust in the S32 Configuration Tool to achieve this?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Appreciate your help—thanks in advance!&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 08 Apr 2025 08:46:08 GMT</pubDate>
    <dc:creator>embedded_will</dc:creator>
    <dc:date>2025-04-08T08:46:08Z</dc:date>
    <item>
      <title>Change CAN Baud Rate in S32K3 Board</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Change-CAN-Baud-Rate-in-S32K3-Board/m-p/2075941#M10203</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi Community,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I'm new to MBDT and working with the S32K344. I'm setting up a basic CAN communication between the S32K344 and CAN Analyzer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The default settings are for 1 Mbps, but I need to run the CAN at 500 kbps. Which parameters should I adjust in the S32 Configuration Tool to achieve this?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Appreciate your help—thanks in advance!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Apr 2025 08:46:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Change-CAN-Baud-Rate-in-S32K3-Board/m-p/2075941#M10203</guid>
      <dc:creator>embedded_will</dc:creator>
      <dc:date>2025-04-08T08:46:08Z</dc:date>
    </item>
    <item>
      <title>Re: Change CAN Baud Rate in S32K3 Board</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Change-CAN-Baud-Rate-in-S32K3-Board/m-p/2086671#M10231</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249069"&gt;@embedded_will&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I would like to point you to an article describing the available options and parameters for configuring CAN peripheral inside S32CT, for S32K344. Here, you could find as well useful information on the Baudrate configuration.&lt;/P&gt;
&lt;P&gt;Please let us know if the information in this article helps, or if further details are required from our side.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/1758456" target="_self"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/1758456&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;Irina&lt;/P&gt;</description>
      <pubDate>Thu, 24 Apr 2025 14:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Change-CAN-Baud-Rate-in-S32K3-Board/m-p/2086671#M10231</guid>
      <dc:creator>Irina_Costachescu</dc:creator>
      <dc:date>2025-04-24T14:21:57Z</dc:date>
    </item>
  </channel>
</rss>