<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K358-Q172 CAN transmission failed in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-Q172-CAN-transmission-failed/m-p/2057261#M10094</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221383"&gt;@Adrian_Gherca&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Forgot to mention that the Can I am using is FlexCAN 6. Many thanks, Xiaomei&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 06 Mar 2025 17:45:53 GMT</pubDate>
    <dc:creator>XH</dc:creator>
    <dc:date>2025-03-06T17:45:53Z</dc:date>
    <item>
      <title>S32K358-Q172 CAN transmission failed</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-Q172-CAN-transmission-failed/m-p/2057251#M10093</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221383"&gt;@Adrian_Gherca&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope you are well. I have built a MBDT Can transmit model mimicking the Can Transmit 342 S32CT example model in the Simulink library. However, when I observe it in Freemaster, the status of the Can_Write module is 2, which means the buffer is full or busy. ( pleas see the attached image). I have also attached the file of my whole model. Could you please help me to see where the issue is? Many thanks, Xiaomei&lt;/P&gt;</description>
      <pubDate>Thu, 06 Mar 2025 17:34:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-Q172-CAN-transmission-failed/m-p/2057251#M10093</guid>
      <dc:creator>XH</dc:creator>
      <dc:date>2025-03-06T17:34:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32K358-Q172 CAN transmission failed</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-Q172-CAN-transmission-failed/m-p/2057261#M10094</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221383"&gt;@Adrian_Gherca&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Forgot to mention that the Can I am using is FlexCAN 6. Many thanks, Xiaomei&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Mar 2025 17:45:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K358-Q172-CAN-transmission-failed/m-p/2057261#M10094</guid>
      <dc:creator>XH</dc:creator>
      <dc:date>2025-03-06T17:45:53Z</dc:date>
    </item>
  </channel>
</rss>