<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 CAN Communication Issue on S32K344 with NXP Model-Based Design Toolbox for S32K3 version 1.6.0</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-Communication-Issue-on-S32K344-with-NXP-Model-Based-Design/m-p/2056781#M10083</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on &lt;STRONG&gt;S32K344&lt;/STRONG&gt; and configuring CAN communication using &lt;STRONG&gt;S32 NXP Model-Based Design Toolbox for S32K3 version 1.6.0&lt;/STRONG&gt;. However, I am facing an issue where I am &lt;STRONG&gt;not receiving any CAN messages&lt;/STRONG&gt; on my CAN analyzer (BusMaster).&lt;/P&gt;&lt;P&gt;I have used the &lt;STRONG&gt;same configuration that was working perfectly in v1.5.0&lt;/STRONG&gt;, but after switching to &lt;STRONG&gt;v1.6.0&lt;/STRONG&gt;, the messages do not appear on the analyzer.&lt;/P&gt;&lt;H3&gt;&lt;STRONG&gt;Details of the Issue:&lt;/STRONG&gt;&lt;/H3&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Setup Details:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Microcontroller: &lt;STRONG&gt;S32K344&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;Development Environment: &lt;STRONG&gt;S32 Design Studio&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;CAN Analyzer: &lt;STRONG&gt;BusMaster&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;Configuration: &lt;STRONG&gt;Same MEX file that worked in v1.5.0&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Steps I have tried:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Verified &lt;STRONG&gt;baud rate and CAN FD settings&lt;/STRONG&gt; (matching the working setup from v1.5.0).&lt;/LI&gt;&lt;LI&gt;Ensured the &lt;STRONG&gt;CAN module initializes without errors&lt;/STRONG&gt;.&lt;/LI&gt;&lt;LI&gt;Checked the &lt;STRONG&gt;message buffer configurations&lt;/STRONG&gt;, which are the same as in v1.5.0.&lt;/LI&gt;&lt;LI&gt;.&lt;/LI&gt;&lt;LI&gt;Verified &lt;STRONG&gt;hardware connections&lt;/STRONG&gt;, ensuring that transceiver and termination resistors are properly in place.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;H3&gt;&lt;STRONG&gt;Request for Assistance:&lt;/STRONG&gt;&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;Is there any &lt;STRONG&gt;known change&lt;/STRONG&gt; in &lt;STRONG&gt;v1.6.0&lt;/STRONG&gt;&amp;nbsp;that could affect CAN transmission/reception?&lt;/LI&gt;&lt;LI&gt;Do I need to modify any &lt;STRONG&gt;additional settings&lt;/STRONG&gt; to get CAN communication working in this version?&lt;/LI&gt;&lt;LI&gt;Are there any &lt;STRONG&gt;debugging steps&lt;/STRONG&gt; recommended to further diagnose this issue?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;For reference, I am attaching my &lt;STRONG&gt;MEX file&lt;/STRONG&gt; and ZIP with&amp;nbsp;&lt;STRONG&gt;Simulink SLX file&lt;/STRONG&gt;, which contain the configurations used.&lt;/P&gt;&lt;P&gt;Any guidance would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="MBDT" id="MBDT"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp; &amp;nbsp;&lt;LI-PRODUCT title="S32K344-WB" id="S32K344-WB"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Thu, 06 Mar 2025 07:03:56 GMT</pubDate>
    <dc:creator>oj</dc:creator>
    <dc:date>2025-03-06T07:03:56Z</dc:date>
    <item>
      <title>CAN Communication Issue on S32K344 with NXP Model-Based Design Toolbox for S32K3 version 1.6.0</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-Communication-Issue-on-S32K344-with-NXP-Model-Based-Design/m-p/2056781#M10083</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on &lt;STRONG&gt;S32K344&lt;/STRONG&gt; and configuring CAN communication using &lt;STRONG&gt;S32 NXP Model-Based Design Toolbox for S32K3 version 1.6.0&lt;/STRONG&gt;. However, I am facing an issue where I am &lt;STRONG&gt;not receiving any CAN messages&lt;/STRONG&gt; on my CAN analyzer (BusMaster).&lt;/P&gt;&lt;P&gt;I have used the &lt;STRONG&gt;same configuration that was working perfectly in v1.5.0&lt;/STRONG&gt;, but after switching to &lt;STRONG&gt;v1.6.0&lt;/STRONG&gt;, the messages do not appear on the analyzer.&lt;/P&gt;&lt;H3&gt;&lt;STRONG&gt;Details of the Issue:&lt;/STRONG&gt;&lt;/H3&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Setup Details:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Microcontroller: &lt;STRONG&gt;S32K344&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;Development Environment: &lt;STRONG&gt;S32 Design Studio&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;CAN Analyzer: &lt;STRONG&gt;BusMaster&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;Configuration: &lt;STRONG&gt;Same MEX file that worked in v1.5.0&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Steps I have tried:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Verified &lt;STRONG&gt;baud rate and CAN FD settings&lt;/STRONG&gt; (matching the working setup from v1.5.0).&lt;/LI&gt;&lt;LI&gt;Ensured the &lt;STRONG&gt;CAN module initializes without errors&lt;/STRONG&gt;.&lt;/LI&gt;&lt;LI&gt;Checked the &lt;STRONG&gt;message buffer configurations&lt;/STRONG&gt;, which are the same as in v1.5.0.&lt;/LI&gt;&lt;LI&gt;.&lt;/LI&gt;&lt;LI&gt;Verified &lt;STRONG&gt;hardware connections&lt;/STRONG&gt;, ensuring that transceiver and termination resistors are properly in place.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;H3&gt;&lt;STRONG&gt;Request for Assistance:&lt;/STRONG&gt;&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;Is there any &lt;STRONG&gt;known change&lt;/STRONG&gt; in &lt;STRONG&gt;v1.6.0&lt;/STRONG&gt;&amp;nbsp;that could affect CAN transmission/reception?&lt;/LI&gt;&lt;LI&gt;Do I need to modify any &lt;STRONG&gt;additional settings&lt;/STRONG&gt; to get CAN communication working in this version?&lt;/LI&gt;&lt;LI&gt;Are there any &lt;STRONG&gt;debugging steps&lt;/STRONG&gt; recommended to further diagnose this issue?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;For reference, I am attaching my &lt;STRONG&gt;MEX file&lt;/STRONG&gt; and ZIP with&amp;nbsp;&lt;STRONG&gt;Simulink SLX file&lt;/STRONG&gt;, which contain the configurations used.&lt;/P&gt;&lt;P&gt;Any guidance would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="MBDT" id="MBDT"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp; &amp;nbsp;&lt;LI-PRODUCT title="S32K344-WB" id="S32K344-WB"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 06 Mar 2025 07:03:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/CAN-Communication-Issue-on-S32K344-with-NXP-Model-Based-Design/m-p/2056781#M10083</guid>
      <dc:creator>oj</dc:creator>
      <dc:date>2025-03-06T07:03:56Z</dc:date>
    </item>
  </channel>
</rss>