<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k3:Can in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2056746#M10075</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I already have done those steps and was able to configure those appropriate pins.&lt;/P&gt;&lt;P&gt;You are again giving excuses. Please pin point the issue by going through it and trying it yourself.&lt;/P&gt;&lt;P&gt;Again it is your duty to solve the problem with the project that I have attached.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 06 Mar 2025 05:56:50 GMT</pubDate>
    <dc:creator>avinashstarkenn</dc:creator>
    <dc:date>2025-03-06T05:56:50Z</dc:date>
    <item>
      <title>S32k3:Can</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2048950#M10011</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have tried to configure CAN0,CAN1,CAN2 on S32k312(100 pins).&lt;/P&gt;&lt;P&gt;I am using model based design tool box&lt;/P&gt;&lt;P&gt;CAN1 and CAN 2 are running successfully with no issues.&lt;/P&gt;&lt;P&gt;CAN0 is not working. I went through all parameters .But all parameters on CAN0 is identical to CAN1.These should not be any issues.&lt;/P&gt;&lt;P&gt;Please solve the issue&lt;/P&gt;&lt;P&gt;CAN transreceiver is not an issue.It is working fine&lt;/P&gt;&lt;P&gt;Attaching the model&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 09:22:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2048950#M10011</guid>
      <dc:creator>avinashstarkenn</dc:creator>
      <dc:date>2025-02-21T09:22:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32k3:Can</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2053021#M10037</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221165"&gt;@avinashstarkenn&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I opened the model you attached and noticed you are using the PTC2 and PTC3 pins for the CAN0 instance. Have you tried assigning different pins for the CAN0_RX and CAN0_TX signals? Or is there any specific reason for why these pins have been chosen for CAN0?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In the default configuration we provide for S32K312 Q172 and S32K311 Q100, the default pins for CAN0_RX and CAN0_TX are set to PTA6 and PTA7.&lt;/P&gt;
&lt;P&gt;I tested these pins on the S32K312-Q172 and S32K311-Q100 and did not encounter any problems in using the CAN Communication.&lt;/P&gt;
&lt;P&gt;Could you provide any more details that could be useful on trying to diagnose this issue?&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Robert V&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 14:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2053021#M10037</guid>
      <dc:creator>robertv</dc:creator>
      <dc:date>2025-02-27T14:29:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32k3:Can</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2053031#M10038</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219933"&gt;@robertv&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I want my CAN pins on PTC2 and PTC3.My custom board is having pins for CAN0.&lt;/P&gt;&lt;P&gt;I was furious when I read you reply. I know that PTA6 and PTA7 will work as those are example code ,but I don't want that.&lt;/P&gt;&lt;P&gt;As NXP has provided CAN0 in PTC2 and PTC3,so it is your duty to solve this problem instead of giving excuses&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 14:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2053031#M10038</guid>
      <dc:creator>avinashstarkenn</dc:creator>
      <dc:date>2025-02-27T14:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32k3:Can</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2053659#M10042</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221165"&gt;@avinashstarkenn&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&lt;SPAN data-teams="true"&gt;The examples and default configuration projects that we provide inside the Model-Based Design Toolbox aim to address specific boards, that we have used for development and testing. As for S32K312, the default configuration is designed to match the S32K312-Q172EVB hardware particularities.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;If you are developing a custom PCB, you would need to reroute the pins according to your hardware schematics. To help with this process, we provide you with a series of articles that showcase the process of creating custom configurations (including CAN configuration):&amp;nbsp;&lt;BR /&gt;- &lt;STRONG&gt;Dio&lt;/STRONG&gt;:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Interacting-with-Digital-Inputs-Outputs-on-MR-CANHUBK344/ta-p/1746789" target="_self"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Interacting-with-Digital-Inputs-Outputs-on-MR-CANHUBK344/ta-p/1746789&lt;/A&gt;&lt;BR /&gt;- &lt;STRONG&gt;UART &amp;amp; FreeMASTER&lt;/STRONG&gt;:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Sending-data-via-UART-and-monitoring-signals-with-FreeMASTER/ta-p/1747896" target="_self"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Sending-data-via-UART-and-monitoring-signals-with-FreeMASTER/ta-p/1747896&lt;/A&gt;&lt;BR /&gt;- &lt;STRONG&gt;ADC &amp;amp; PWM&lt;/STRONG&gt;:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Controlling-LED-intensity-with-ADC-and-PWM/ta-p/1747898" target="_self"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Controlling-LED-intensity-with-ADC-and-PWM/ta-p/1747898&lt;/A&gt;&lt;BR /&gt;- &lt;STRONG&gt;CAN&lt;/STRONG&gt;:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/1758456" target="_self"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/1758456&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Robert V&lt;/P&gt;</description>
      <pubDate>Fri, 28 Feb 2025 09:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2053659#M10042</guid>
      <dc:creator>robertv</dc:creator>
      <dc:date>2025-02-28T09:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32k3:Can</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2056746#M10075</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I already have done those steps and was able to configure those appropriate pins.&lt;/P&gt;&lt;P&gt;You are again giving excuses. Please pin point the issue by going through it and trying it yourself.&lt;/P&gt;&lt;P&gt;Again it is your duty to solve the problem with the project that I have attached.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 06 Mar 2025 05:56:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32k3-Can/m-p/2056746#M10075</guid>
      <dc:creator>avinashstarkenn</dc:creator>
      <dc:date>2025-03-06T05:56:50Z</dc:date>
    </item>
  </channel>
</rss>