<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックwhere to look for MPC564xL.rbf file ?</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/where-to-look-for-MPC564xL-rbf-file/m-p/599899#M10</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;User manual sasy: "The s-record file that needs to be manually programmed into the MCU is MPC564xL.rbf" and then:&amp;nbsp;&lt;/P&gt;&lt;P&gt;"It is located in the MCD Toolbox installation directory under: ...\tools\BootLoader\RBF_Files."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I see there is no such file in this directory. There is only .rba (RAM) file in the RBA_Files folder. Is it mistake in the User Guide ? How should we prepare/configure board to use it with PIL simulation ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of using .rba file: does it matter if we use MPC564xL.rba or PXS20xx.rba to work with TWR-PXS2010 board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for help&lt;/P&gt;&lt;P&gt;Maciek&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Oct 2016 13:04:21 GMT</pubDate>
    <dc:creator>Maciek</dc:creator>
    <dc:date>2016-10-25T13:04:21Z</dc:date>
    <item>
      <title>where to look for MPC564xL.rbf file ?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/where-to-look-for-MPC564xL-rbf-file/m-p/599899#M10</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;User manual sasy: "The s-record file that needs to be manually programmed into the MCU is MPC564xL.rbf" and then:&amp;nbsp;&lt;/P&gt;&lt;P&gt;"It is located in the MCD Toolbox installation directory under: ...\tools\BootLoader\RBF_Files."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I see there is no such file in this directory. There is only .rba (RAM) file in the RBA_Files folder. Is it mistake in the User Guide ? How should we prepare/configure board to use it with PIL simulation ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In case of using .rba file: does it matter if we use MPC564xL.rba or PXS20xx.rba to work with TWR-PXS2010 board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for help&lt;/P&gt;&lt;P&gt;Maciek&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Oct 2016 13:04:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/where-to-look-for-MPC564xL-rbf-file/m-p/599899#M10</guid>
      <dc:creator>Maciek</dc:creator>
      <dc:date>2016-10-25T13:04:21Z</dc:date>
    </item>
    <item>
      <title>Re: where to look for MPC564xL.rbf file ?</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/where-to-look-for-MPC564xL-rbf-file/m-p/599900#M11</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;- For the MPC564xL there is no RBF file.&amp;nbsp; The for the MPC564xL there is only a RBA file used.&amp;nbsp; &lt;/P&gt;&lt;P&gt;- MPC564xL.rba&amp;nbsp;and PXS20xx.rba are identical and therefore either can be used.&lt;/P&gt;&lt;P&gt;- To prepare the MPC564xL for PIL mode you will need to have the MCU setup for Auto Baud mode.&amp;nbsp; That means that the FAB pin needs to be 1 the ABS2 pin needs to be 1 and the ABS0 pin needs to be 0.&amp;nbsp; Please see the MPC564xL Reference Manual chapter 9 for more details.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Oct 2016 16:00:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/where-to-look-for-MPC564xL-rbf-file/m-p/599900#M11</guid>
      <dc:creator>john_floros</dc:creator>
      <dc:date>2016-10-25T16:00:23Z</dc:date>
    </item>
  </channel>
</rss>