<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE FAQsのトピック16: Target error from status-poll: Ee(02). Not connected to emulator</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/16-Target-error-from-status-poll-Ee-02-Not-connected-to-emulator/m-p/467709#M8</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;During a debug session, whilst your target is executing , the debug tools will poll the target to determine whether it has halted on a breakpoint or event. A "&lt;STRONG&gt;16: Target error from status-poll: Ee(02). Not connected to emulator&lt;/STRONG&gt;" error is returned whenever the debug tools cannot get the present target state. In this case, the debug connection to your MCU is considered offline.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some of the things that could cause this error include:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MCU going into one of the sleep modes.&lt;/LI&gt;&lt;LI&gt;MCU being reset, for example by a watchdog timer.&lt;/LI&gt;&lt;LI&gt;Faulty USB cable or bad USB port&lt;/LI&gt;&lt;LI&gt;Intermittent power to the target (or bad ground).&lt;/LI&gt;&lt;LI&gt;The MCU crystal or a PLL setting could be out of bounds affecting debug communications through the debug access port.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are connecting to the target using a Red Probe+ (but NOT using an LPC-Link), then in the Project Debug Configuration, you can specify a reduced wire speed (i.e. "Maximum wire speed). The default is typically 3 MHz, or 3000 KHz. Setting this value to a lower number, such as 1000 KHz (1 MHz), can sometimes improve matters - though this depends on the actual cause of the status-poll error.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Mar 2016 15:28:29 GMT</pubDate>
    <dc:creator>lpcware-support</dc:creator>
    <dc:date>2016-03-31T15:28:29Z</dc:date>
    <item>
      <title>16: Target error from status-poll: Ee(02). Not connected to emulator</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/16-Target-error-from-status-poll-Ee-02-Not-connected-to-emulator/m-p/467709#M8</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;During a debug session, whilst your target is executing , the debug tools will poll the target to determine whether it has halted on a breakpoint or event. A "&lt;STRONG&gt;16: Target error from status-poll: Ee(02). Not connected to emulator&lt;/STRONG&gt;" error is returned whenever the debug tools cannot get the present target state. In this case, the debug connection to your MCU is considered offline.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some of the things that could cause this error include:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MCU going into one of the sleep modes.&lt;/LI&gt;&lt;LI&gt;MCU being reset, for example by a watchdog timer.&lt;/LI&gt;&lt;LI&gt;Faulty USB cable or bad USB port&lt;/LI&gt;&lt;LI&gt;Intermittent power to the target (or bad ground).&lt;/LI&gt;&lt;LI&gt;The MCU crystal or a PLL setting could be out of bounds affecting debug communications through the debug access port.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are connecting to the target using a Red Probe+ (but NOT using an LPC-Link), then in the Project Debug Configuration, you can specify a reduced wire speed (i.e. "Maximum wire speed). The default is typically 3 MHz, or 3000 KHz. Setting this value to a lower number, such as 1000 KHz (1 MHz), can sometimes improve matters - though this depends on the actual cause of the status-poll error.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Mar 2016 15:28:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/16-Target-error-from-status-poll-Ee-02-Not-connected-to-emulator/m-p/467709#M8</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-03-31T15:28:29Z</dc:date>
    </item>
  </channel>
</rss>