<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE FAQsのトピック02: Failed on connect: Ep(01). Target marked as not debuggable</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/02-Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/467619#M5</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the error "&lt;STRONG&gt;02: Failed on connect: Ep(01). Target marked as not debuggable&lt;/STRONG&gt;" is seen when trying to start a debug connection, this normally means one of:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The cable between the debug probe (e.g. Red Probe+, LPC-Link) is not correctly inserted, or is broken.&lt;UL&gt;&lt;LI&gt;In particular make sure that pin 1 of the cable is connected to pin 1 of the header on the board (most cables have a red stripe to indicate pin 1)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;The board is not provided with power.&lt;/LI&gt;&lt;LI&gt;The board's debug circuit is incorrectly designed.&lt;UL&gt;&lt;LI&gt;For more information see the FAQ "&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="388998" data-objecttype="1" href="https://community.nxp.com/thread/388998"&gt;&lt;EM&gt;&lt;STRONG&gt;Design Considerations for Debug&lt;/STRONG&gt;&lt;/EM&gt;&lt;/A&gt;".&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;The target MCU has been put into a &lt;STRONG&gt;flash protection mode&lt;/STRONG&gt; via CRP (Code Read Protect).&lt;UL&gt;&lt;LI&gt;For more information see the FAQ "&lt;A href="https://community.nxp.com/thread/388983"&gt;Code Read Protection (CRP)&lt;/A&gt; ".&lt;/LI&gt;&lt;LI&gt;It may be possible to recover this using &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.flashmagictool.com%2F"&gt;FlashMagic&lt;/A&gt; over a UART/USB (depending upon the MCU).&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;An application has been programmed into the MCU which reconfigures the &lt;STRONG&gt;debug pins&lt;/STRONG&gt; for other uses or has &lt;STRONG&gt;programmed the clock&lt;/STRONG&gt; into a "strange state".&lt;UL&gt;&lt;LI&gt;It may be possible to recover from this by booting into ISP mode or enabling "vector catch" functionality. For more details, please see the FAQ "&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389112" data-objecttype="1" href="https://community.nxp.com/thread/389112"&gt;&lt;STRONG&gt;Regaining debug access to target MCU&lt;/STRONG&gt;&lt;/A&gt;".&lt;/LI&gt;&lt;LI&gt;Alternatively, you may be able to use &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.flashmagictool.com%2F"&gt;FlashMagic&lt;/A&gt; to erase the flash.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Mar 2016 15:25:21 GMT</pubDate>
    <dc:creator>lpcware-support</dc:creator>
    <dc:date>2016-03-31T15:25:21Z</dc:date>
    <item>
      <title>02: Failed on connect: Ep(01). Target marked as not debuggable</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/02-Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/467619#M5</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the error "&lt;STRONG&gt;02: Failed on connect: Ep(01). Target marked as not debuggable&lt;/STRONG&gt;" is seen when trying to start a debug connection, this normally means one of:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;The cable between the debug probe (e.g. Red Probe+, LPC-Link) is not correctly inserted, or is broken.&lt;UL&gt;&lt;LI&gt;In particular make sure that pin 1 of the cable is connected to pin 1 of the header on the board (most cables have a red stripe to indicate pin 1)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;The board is not provided with power.&lt;/LI&gt;&lt;LI&gt;The board's debug circuit is incorrectly designed.&lt;UL&gt;&lt;LI&gt;For more information see the FAQ "&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="388998" data-objecttype="1" href="https://community.nxp.com/thread/388998"&gt;&lt;EM&gt;&lt;STRONG&gt;Design Considerations for Debug&lt;/STRONG&gt;&lt;/EM&gt;&lt;/A&gt;".&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;The target MCU has been put into a &lt;STRONG&gt;flash protection mode&lt;/STRONG&gt; via CRP (Code Read Protect).&lt;UL&gt;&lt;LI&gt;For more information see the FAQ "&lt;A href="https://community.nxp.com/thread/388983"&gt;Code Read Protection (CRP)&lt;/A&gt; ".&lt;/LI&gt;&lt;LI&gt;It may be possible to recover this using &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.flashmagictool.com%2F"&gt;FlashMagic&lt;/A&gt; over a UART/USB (depending upon the MCU).&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;An application has been programmed into the MCU which reconfigures the &lt;STRONG&gt;debug pins&lt;/STRONG&gt; for other uses or has &lt;STRONG&gt;programmed the clock&lt;/STRONG&gt; into a "strange state".&lt;UL&gt;&lt;LI&gt;It may be possible to recover from this by booting into ISP mode or enabling "vector catch" functionality. For more details, please see the FAQ "&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389112" data-objecttype="1" href="https://community.nxp.com/thread/389112"&gt;&lt;STRONG&gt;Regaining debug access to target MCU&lt;/STRONG&gt;&lt;/A&gt;".&lt;/LI&gt;&lt;LI&gt;Alternatively, you may be able to use &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.flashmagictool.com%2F"&gt;FlashMagic&lt;/A&gt; to erase the flash.&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Mar 2016 15:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/02-Failed-on-connect-Ep-01-Target-marked-as-not-debuggable/m-p/467619#M5</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-03-31T15:25:21Z</dc:date>
    </item>
  </channel>
</rss>