<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Debugging a running system in LPCXpresso IDE FAQs</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Debugging-a-running-system/m-p/469524#M43</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is possible to debug a running system, without loading an application. To do this, you will need a project with a valid application (.axf file), although it will not be downloaded. If the image that the target is running matches the image in the project, then debug symbols will be available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You then need to modify the launch configuration for the project such that the &lt;STRONG&gt;Attach Only&lt;/STRONG&gt; option is set to "True".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For details of how to create/edit launch configurations, please see the FAQ:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389073" data-objecttype="1" href="https://community.nxp.com/thread/389073"&gt;Launch Configuration Menu&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Mar 2016 18:16:16 GMT</pubDate>
    <dc:creator>lpcware-support</dc:creator>
    <dc:date>2016-03-31T18:16:16Z</dc:date>
    <item>
      <title>Debugging a running system</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Debugging-a-running-system/m-p/469524#M43</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is possible to debug a running system, without loading an application. To do this, you will need a project with a valid application (.axf file), although it will not be downloaded. If the image that the target is running matches the image in the project, then debug symbols will be available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You then need to modify the launch configuration for the project such that the &lt;STRONG&gt;Attach Only&lt;/STRONG&gt; option is set to "True".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For details of how to create/edit launch configurations, please see the FAQ:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389073" data-objecttype="1" href="https://community.nxp.com/thread/389073"&gt;Launch Configuration Menu&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Mar 2016 18:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Debugging-a-running-system/m-p/469524#M43</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-03-31T18:16:16Z</dc:date>
    </item>
  </channel>
</rss>