<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE FAQs中的主题 Re: LPCXpresso code build through Command</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/LPCXpresso-code-build-through-Command/m-p/1492347#M194</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199410"&gt;@ankitvats&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;you have many options:&lt;/P&gt;&lt;P&gt;a) simple create batch file and call the compiler and linker. Easy for simple projects.&lt;/P&gt;&lt;P&gt;b) use a make file and call it with make (or cmake, if you prefer), see for example &lt;A href="https://mcuoneclipse.com/2017/07/22/tutorial-makefile-projects-with-eclipse/" target="_blank"&gt;https://mcuoneclipse.com/2017/07/22/tutorial-makefile-projects-with-eclipse/&lt;/A&gt; or &lt;A href="https://mcuoneclipse.com/2012/02/13/make-my-make-with-eclipse-and-mcu10/" target="_blank"&gt;https://mcuoneclipse.com/2012/02/13/make-my-make-with-eclipse-and-mcu10/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;c) call the IDE to build your project from the command line, see &lt;A href="https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-line/" target="_blank"&gt;https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-line/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;d) if using the MCUXpresso SDK, you can do it directly too, see &lt;A href="https://mcuoneclipse.com/2019/04/14/tutorial-mcuxpresso-sdk-with-linux-part-1-installation-and-build/" target="_blank"&gt;https://mcuoneclipse.com/2019/04/14/tutorial-mcuxpresso-sdk-with-linux-part-1-installation-and-build/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
    <pubDate>Wed, 20 Jul 2022 09:42:30 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2022-07-20T09:42:30Z</dc:date>
    <item>
      <title>LPCXpresso code build through Command</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/LPCXpresso-code-build-through-Command/m-p/1492314#M193</link>
      <description>&lt;P&gt;Hi , I wants to Build by Firmware through cmd that generate .bin and .hex file in Window system&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So , How to do that ??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 09:15:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/LPCXpresso-code-build-through-Command/m-p/1492314#M193</guid>
      <dc:creator>ankitvats</dc:creator>
      <dc:date>2022-07-20T09:15:10Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso code build through Command</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/LPCXpresso-code-build-through-Command/m-p/1492347#M194</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199410"&gt;@ankitvats&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;you have many options:&lt;/P&gt;&lt;P&gt;a) simple create batch file and call the compiler and linker. Easy for simple projects.&lt;/P&gt;&lt;P&gt;b) use a make file and call it with make (or cmake, if you prefer), see for example &lt;A href="https://mcuoneclipse.com/2017/07/22/tutorial-makefile-projects-with-eclipse/" target="_blank"&gt;https://mcuoneclipse.com/2017/07/22/tutorial-makefile-projects-with-eclipse/&lt;/A&gt; or &lt;A href="https://mcuoneclipse.com/2012/02/13/make-my-make-with-eclipse-and-mcu10/" target="_blank"&gt;https://mcuoneclipse.com/2012/02/13/make-my-make-with-eclipse-and-mcu10/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;c) call the IDE to build your project from the command line, see &lt;A href="https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-line/" target="_blank"&gt;https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-line/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;d) if using the MCUXpresso SDK, you can do it directly too, see &lt;A href="https://mcuoneclipse.com/2019/04/14/tutorial-mcuxpresso-sdk-with-linux-part-1-installation-and-build/" target="_blank"&gt;https://mcuoneclipse.com/2019/04/14/tutorial-mcuxpresso-sdk-with-linux-part-1-installation-and-build/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Wed, 20 Jul 2022 09:42:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/LPCXpresso-code-build-through-Command/m-p/1492347#M194</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2022-07-20T09:42:30Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso code build through Command</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/LPCXpresso-code-build-through-Command/m-p/1493285#M196</link>
      <description>&lt;P&gt;Thanks for your support.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jul 2022 10:56:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/LPCXpresso-code-build-through-Command/m-p/1493285#M196</guid>
      <dc:creator>ankitvats</dc:creator>
      <dc:date>2022-07-21T10:56:08Z</dc:date>
    </item>
  </channel>
</rss>