<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE FAQs中的主题 Debugger disconnect behavior</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Debugger-disconnect-behavior/m-p/586493#M155</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When the debugger disconnects from the target, you control the behavior of the target processor using the process described below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Select the project in the Project Explorer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Project.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37055i094052188A933201/image-size/large?v=v2&amp;amp;px=999" role="button" title="Project.png" alt="Project.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Refer to the following FAQ to select the Launch Configuration setting for the project&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="https://community.nxp.com/thread/389073"&gt;Launch Configuration Menu&lt;/A&gt; &lt;/P&gt;&lt;P&gt;3. Ensure you are editing the setting for your project&lt;/P&gt;&lt;P&gt;4. In the right-hand section, ensure the Debugger tab is selected&lt;/P&gt;&lt;P&gt;5. Ensure you have selected the Target Configuration settings&lt;/P&gt;&lt;P&gt;6. Locate the Disconnect behavior settings and select the desired option from the drop down list.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Project_disconnect.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37528i8A58292D04DBD655/image-size/large?v=v2&amp;amp;px=999" role="button" title="Project_disconnect.png" alt="Project_disconnect.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P class="line874"&gt;&lt;/P&gt;&lt;P class="line874"&gt;Four options are supported: &lt;SPAN class="anchor"&gt;&lt;/SPAN&gt;&lt;SPAN class="anchor"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;nochange - leave the processor exactly as it is (if it was running, leave it running, if it was stopped, leave it stopped) &lt;/LI&gt;&lt;LI&gt;stop - stop the processor &lt;/LI&gt;&lt;LI&gt;cont - (continue) run the program from the current point &lt;/LI&gt;&lt;LI&gt;run_cont - run the program from the start (simulated reset) &lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jul 2016 10:23:03 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2016-07-19T10:23:03Z</dc:date>
    <item>
      <title>Debugger disconnect behavior</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Debugger-disconnect-behavior/m-p/586493#M155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When the debugger disconnects from the target, you control the behavior of the target processor using the process described below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Select the project in the Project Explorer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Project.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37055i094052188A933201/image-size/large?v=v2&amp;amp;px=999" role="button" title="Project.png" alt="Project.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Refer to the following FAQ to select the Launch Configuration setting for the project&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="https://community.nxp.com/thread/389073"&gt;Launch Configuration Menu&lt;/A&gt; &lt;/P&gt;&lt;P&gt;3. Ensure you are editing the setting for your project&lt;/P&gt;&lt;P&gt;4. In the right-hand section, ensure the Debugger tab is selected&lt;/P&gt;&lt;P&gt;5. Ensure you have selected the Target Configuration settings&lt;/P&gt;&lt;P&gt;6. Locate the Disconnect behavior settings and select the desired option from the drop down list.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Project_disconnect.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37528i8A58292D04DBD655/image-size/large?v=v2&amp;amp;px=999" role="button" title="Project_disconnect.png" alt="Project_disconnect.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P class="line874"&gt;&lt;/P&gt;&lt;P class="line874"&gt;Four options are supported: &lt;SPAN class="anchor"&gt;&lt;/SPAN&gt;&lt;SPAN class="anchor"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;nochange - leave the processor exactly as it is (if it was running, leave it running, if it was stopped, leave it stopped) &lt;/LI&gt;&lt;LI&gt;stop - stop the processor &lt;/LI&gt;&lt;LI&gt;cont - (continue) run the program from the current point &lt;/LI&gt;&lt;LI&gt;run_cont - run the program from the start (simulated reset) &lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2016 10:23:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Debugger-disconnect-behavior/m-p/586493#M155</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-07-19T10:23:03Z</dc:date>
    </item>
  </channel>
</rss>