<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE FAQs中的主题 What are none, nohost and semihost libraries?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/What-are-none-nohost-and-semihost-libraries/m-p/475327#M141</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPCXpresso is supplied with several 'stubs' that form the very bottom of the C library and include certain low-level functions used by other functions in the library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each C library (Redlib and Newlib) is provided in three variants, with each variant providing a differing set of these stubs, and hence providing differing levels of functionality. The libraries are named as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Redlib (none)&lt;/LI&gt;&lt;LI&gt;Redlib (nohost)&lt;/LI&gt;&lt;LI&gt;Redlib (semihost)&lt;/LI&gt;&lt;LI&gt;Newlib (none)&lt;/LI&gt;&lt;LI&gt;Newlib (nohost)&lt;/LI&gt;&lt;LI&gt;Newlib (semihost)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The functionality provided in each variant is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Semihost&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This library variant provides implementation of all functions, including file I/O. The file I/O will be directed through the debugger and will be performed on the host system (semihosting). For example, printf/scanf will use the debugger console window and fread/fwrite will operate on files on the host system. Note that this emulated I/O is slow and can only be used when debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Nohost&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This library variant provides the string and memory handling functions and some file-based I/O functions. However, it assumes that you have no debugging host system, thus any file I/O will do nothing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;None&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is literally no stub and has the smallest memory footprint. It excludes low-level functions for all file-based I/O and some string and memory handling functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In many embedded microcontroller applications it is possible to use the None variant (ie no low level stubs) by careful use of the C library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;For more information...&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389140" data-objecttype="1" href="https://community.nxp.com/thread/389140"&gt;Using printf()&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389156" data-objecttype="1" href="https://community.nxp.com/thread/389156"&gt;What is Semihosting?&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Apr 2016 05:41:08 GMT</pubDate>
    <dc:creator>lpcware-support</dc:creator>
    <dc:date>2016-04-01T05:41:08Z</dc:date>
    <item>
      <title>What are none, nohost and semihost libraries?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/What-are-none-nohost-and-semihost-libraries/m-p/475327#M141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPCXpresso is supplied with several 'stubs' that form the very bottom of the C library and include certain low-level functions used by other functions in the library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Each C library (Redlib and Newlib) is provided in three variants, with each variant providing a differing set of these stubs, and hence providing differing levels of functionality. The libraries are named as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Redlib (none)&lt;/LI&gt;&lt;LI&gt;Redlib (nohost)&lt;/LI&gt;&lt;LI&gt;Redlib (semihost)&lt;/LI&gt;&lt;LI&gt;Newlib (none)&lt;/LI&gt;&lt;LI&gt;Newlib (nohost)&lt;/LI&gt;&lt;LI&gt;Newlib (semihost)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The functionality provided in each variant is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Semihost&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This library variant provides implementation of all functions, including file I/O. The file I/O will be directed through the debugger and will be performed on the host system (semihosting). For example, printf/scanf will use the debugger console window and fread/fwrite will operate on files on the host system. Note that this emulated I/O is slow and can only be used when debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Nohost&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This library variant provides the string and memory handling functions and some file-based I/O functions. However, it assumes that you have no debugging host system, thus any file I/O will do nothing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;None&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is literally no stub and has the smallest memory footprint. It excludes low-level functions for all file-based I/O and some string and memory handling functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In many embedded microcontroller applications it is possible to use the None variant (ie no low level stubs) by careful use of the C library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;For more information...&lt;/SPAN&gt;&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389140" data-objecttype="1" href="https://community.nxp.com/thread/389140"&gt;Using printf()&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389156" data-objecttype="1" href="https://community.nxp.com/thread/389156"&gt;What is Semihosting?&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Apr 2016 05:41:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/What-are-none-nohost-and-semihost-libraries/m-p/475327#M141</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-04-01T05:41:08Z</dc:date>
    </item>
  </channel>
</rss>