<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE FAQs中的主题 Using an LPC-Link2 as an LPC4370 evaluation board</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Using-an-LPC-Link2-as-an-LPC4370-evaluation-board/m-p/474917#M130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As well as being a standalone debug probe, the &lt;A _jive_internal="true" class="" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fmicrocontrollers-and-processors%2Farm-processors%2Flpc-cortex-m-mcus%2Flpc-low-power-cortex-m4-mcus%2Flpc4300-cortex-m4-m0-mcus%2Flpc-link2%3AOM13054"&gt;LPC-Link2&lt;/A&gt; can also be used as a simple LPC4370 evaluation board. The following notes may assist in such usage.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Debug connection&lt;/SPAN&gt;&lt;/H2&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Make sure that you have connected the JTAG/SWD cable from your debug probe to the target LPC-Link2's connector J2 (and not J7!). Thus if you are using a two LPC-Link2s, one as the debug probe and one as the target - you need to connect J7 on the debug probe to J2 on the target.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Flash Memory&lt;/SPAN&gt;&lt;/H2&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The LPC-Link2 has a 1 MB SPIFI flash (Winbond W25Q80BVSSIG) mounted on it (at address 0x14000000). You can program this in LPCXpresso using the "&lt;STRONG&gt;LPC18_43_SPIFI_GENERIC.cfx&lt;/STRONG&gt;" flash driver. Make sure that you have a jumper fitted to JP1 though. The XML file in the attached &lt;STRONG&gt;LPC4370-Link2-M4only.zip&lt;/STRONG&gt; can be used to set up the memory configuration of your project for this memory/flash driver.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Power&lt;/SPAN&gt;&lt;/H2&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If powering the target LPC-Link2 via USB, then we would normally suggest doing this from a powered USB hub that is not connected to your PC. This will prevent any chance of the target LPC-Link2 being seen by the tools running on the PC as a usable debug probe. If debugging the target LPC-Link2 using another LPC-Link2, then you can supply power from the debug LPC-Link2 if you fit jumper JP2 (though this is not generally recommended if you have additional hardware attached to the target LPC-Link2).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Simple example application&lt;/SPAN&gt;&lt;/H2&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A simple blinky application for the LPC4370/LPC-Link2 can be found in the attached &lt;STRONG&gt;LPC4370_LPCLink2_LEDblinky.zip.&lt;/STRONG&gt; Download and save the zipfile to your local disk, then use the LPCXpresso "Quickstart Panel -&amp;gt; Import project(s)" option to import it into your workspace. In order to build this, you will also need to import the &lt;STRONG&gt;CMSIS_LPC43xx_DriverLib&lt;/STRONG&gt; library project from the LPCXpresso examples into your workspace. For details of importing, building and debugging projects - please see the LPCXpresso User Guide, provided within the product itself.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The LPC-Link2 is also a supported target board for our LPCOpen software platform. You can download example code from our &lt;A _jive_internal="true" class="" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fhardware-development-tools%2Flpcxpresso-boards%2Flpcopen-software-for-lpc43xx%3ALPCOPEN-SOFTWARE-FOR-LPC43XX"&gt;LPCOpen pages&lt;/A&gt;.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;For more information...&lt;/SPAN&gt;&lt;/H2&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For more information on debugging and developing LPC43xx applications in LPCXpresso, please see the FAQ "&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389077" data-objecttype="1" href="https://community.nxp.com/thread/389077"&gt;LPC18 / LPC43 support in LPCXpresso&lt;/A&gt; "&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For more information on the LPC-Link2, please visit &lt;A _jive_internal="true" class="" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fmicrocontrollers-and-processors%2Farm-processors%2Flpc-cortex-m-mcus%2Flpc-low-power-cortex-m4-mcus%2Flpc4300-cortex-m4-m0-mcus%2Flpc-link2%3AOM13054"&gt;here.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338849"&gt;LPC4370-Link2-M4only.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338849"&gt;LPC4370_LPCLink2_LEDblinky.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Apr 2016 04:51:41 GMT</pubDate>
    <dc:creator>lpcware-support</dc:creator>
    <dc:date>2016-04-01T04:51:41Z</dc:date>
    <item>
      <title>Using an LPC-Link2 as an LPC4370 evaluation board</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Using-an-LPC-Link2-as-an-LPC4370-evaluation-board/m-p/474917#M130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As well as being a standalone debug probe, the &lt;A _jive_internal="true" class="" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fmicrocontrollers-and-processors%2Farm-processors%2Flpc-cortex-m-mcus%2Flpc-low-power-cortex-m4-mcus%2Flpc4300-cortex-m4-m0-mcus%2Flpc-link2%3AOM13054"&gt;LPC-Link2&lt;/A&gt; can also be used as a simple LPC4370 evaluation board. The following notes may assist in such usage.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Debug connection&lt;/SPAN&gt;&lt;/H2&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Make sure that you have connected the JTAG/SWD cable from your debug probe to the target LPC-Link2's connector J2 (and not J7!). Thus if you are using a two LPC-Link2s, one as the debug probe and one as the target - you need to connect J7 on the debug probe to J2 on the target.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Flash Memory&lt;/SPAN&gt;&lt;/H2&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The LPC-Link2 has a 1 MB SPIFI flash (Winbond W25Q80BVSSIG) mounted on it (at address 0x14000000). You can program this in LPCXpresso using the "&lt;STRONG&gt;LPC18_43_SPIFI_GENERIC.cfx&lt;/STRONG&gt;" flash driver. Make sure that you have a jumper fitted to JP1 though. The XML file in the attached &lt;STRONG&gt;LPC4370-Link2-M4only.zip&lt;/STRONG&gt; can be used to set up the memory configuration of your project for this memory/flash driver.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Power&lt;/SPAN&gt;&lt;/H2&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If powering the target LPC-Link2 via USB, then we would normally suggest doing this from a powered USB hub that is not connected to your PC. This will prevent any chance of the target LPC-Link2 being seen by the tools running on the PC as a usable debug probe. If debugging the target LPC-Link2 using another LPC-Link2, then you can supply power from the debug LPC-Link2 if you fit jumper JP2 (though this is not generally recommended if you have additional hardware attached to the target LPC-Link2).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;Simple example application&lt;/SPAN&gt;&lt;/H2&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A simple blinky application for the LPC4370/LPC-Link2 can be found in the attached &lt;STRONG&gt;LPC4370_LPCLink2_LEDblinky.zip.&lt;/STRONG&gt; Download and save the zipfile to your local disk, then use the LPCXpresso "Quickstart Panel -&amp;gt; Import project(s)" option to import it into your workspace. In order to build this, you will also need to import the &lt;STRONG&gt;CMSIS_LPC43xx_DriverLib&lt;/STRONG&gt; library project from the LPCXpresso examples into your workspace. For details of importing, building and debugging projects - please see the LPCXpresso User Guide, provided within the product itself.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The LPC-Link2 is also a supported target board for our LPCOpen software platform. You can download example code from our &lt;A _jive_internal="true" class="" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fsoftware-and-tools%2Fhardware-development-tools%2Flpcxpresso-boards%2Flpcopen-software-for-lpc43xx%3ALPCOPEN-SOFTWARE-FOR-LPC43XX"&gt;LPCOpen pages&lt;/A&gt;.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;H2&gt;&lt;SPAN style="color: #eb7a3d;"&gt;For more information...&lt;/SPAN&gt;&lt;/H2&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For more information on debugging and developing LPC43xx applications in LPCXpresso, please see the FAQ "&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389077" data-objecttype="1" href="https://community.nxp.com/thread/389077"&gt;LPC18 / LPC43 support in LPCXpresso&lt;/A&gt; "&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For more information on the LPC-Link2, please visit &lt;A _jive_internal="true" class="" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fproducts%2Fmicrocontrollers-and-processors%2Farm-processors%2Flpc-cortex-m-mcus%2Flpc-low-power-cortex-m4-mcus%2Flpc4300-cortex-m4-m0-mcus%2Flpc-link2%3AOM13054"&gt;here.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338849"&gt;LPC4370-Link2-M4only.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338849"&gt;LPC4370_LPCLink2_LEDblinky.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Apr 2016 04:51:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Using-an-LPC-Link2-as-an-LPC4370-evaluation-board/m-p/474917#M130</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-04-01T04:51:41Z</dc:date>
    </item>
  </channel>
</rss>