<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problems compiling &amp;quot;__attribute__((at&amp;quot; in LPCXpresso IDE FAQs</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Problems-compiling-quot-attribute-at-quot/m-p/473959#M113</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Some other toolchains provide a compiler extension &lt;STRONG&gt;__attribute__((at(addr)))&lt;/STRONG&gt; which acts as a request that the variable that it is applied to is placed at location addr. For example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;&lt;STRONG&gt;&lt;CODE&gt;static HostController _controller __attribute__((at(USB_RAM_BASE)));&lt;/CODE&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;&lt;/P&gt;&lt;P&gt;The GNU toolchain as used by the LPCXpresso IDE provides no direct equivalent of this '&lt;STRONG&gt;at&lt;/STRONG&gt;' attribute.&lt;/P&gt;&lt;P&gt;Often the 'at' attribute is being used to simply place a buffer variable into a specific bank of RAM. This will often be possible just using the section macros provided in the header &lt;STRONG&gt;cr_section_macros.h&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more information, please see the FAQ "&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389101" data-objecttype="1" href="https://community.nxp.com/thread/389101"&gt;Placing data at an address&lt;/A&gt;".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Mar 2016 22:51:56 GMT</pubDate>
    <dc:creator>lpcware-support</dc:creator>
    <dc:date>2016-03-31T22:51:56Z</dc:date>
    <item>
      <title>Problems compiling "__attribute__((at"</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Problems-compiling-quot-attribute-at-quot/m-p/473959#M113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Some other toolchains provide a compiler extension &lt;STRONG&gt;__attribute__((at(addr)))&lt;/STRONG&gt; which acts as a request that the variable that it is applied to is placed at location addr. For example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier new,courier;"&gt;&lt;STRONG&gt;&lt;CODE&gt;static HostController _controller __attribute__((at(USB_RAM_BASE)));&lt;/CODE&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #646464; font-family: Arial, sans-serif; font-size: 12px;"&gt;&lt;/P&gt;&lt;P&gt;The GNU toolchain as used by the LPCXpresso IDE provides no direct equivalent of this '&lt;STRONG&gt;at&lt;/STRONG&gt;' attribute.&lt;/P&gt;&lt;P&gt;Often the 'at' attribute is being used to simply place a buffer variable into a specific bank of RAM. This will often be possible just using the section macros provided in the header &lt;STRONG&gt;cr_section_macros.h&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more information, please see the FAQ "&lt;A _jive_internal="true" data-containerid="11529" data-containertype="14" data-objectid="389101" data-objecttype="1" href="https://community.nxp.com/thread/389101"&gt;Placing data at an address&lt;/A&gt;".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Mar 2016 22:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Problems-compiling-quot-attribute-at-quot/m-p/473959#M113</guid>
      <dc:creator>lpcware-support</dc:creator>
      <dc:date>2016-03-31T22:51:56Z</dc:date>
    </item>
  </channel>
</rss>