<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ee(02) on custom board after programming sample UART code in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Ee-02-on-custom-board-after-programming-sample-UART-code/m-p/545994#M9472</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by victorpau on Tue Jul 20 05:48:09 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I found the problem. It seems that while I was programming the chip I activated accidentally the CRP3, so the LPC1114 is completely isolated now. I've been using other micro-controllers before and I was expecting that the protection only avoided other people to read the code, not myself to program it again (As it's called Code Read Protection I didn't expect it to avoid writing)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So I think the only way that I have is to change the chip from the board for a new one, isn't it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It would be nice if LPCXpresso showed some warning when you choose to program the device with CRP3 so people doesn't do it by mistake.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Victor Pau&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:00:18 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:00:18Z</dc:date>
    <item>
      <title>Ee(02) on custom board after programming sample UART code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Ee-02-on-custom-board-after-programming-sample-UART-code/m-p/545992#M9470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by victorpau on Mon Jul 12 00:29:20 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've been developing and debugging some code with LPCXpresso for a custom board with a LPC1114/201. I was programming it many time and it was working great, but then I programmed both of my custom boards with different code for a test, and I cannot program them anymore. (But I can programm the sample LPC1114/301 that comes with the LPC-Link)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC1114/201 is working properly (I can test in my custom board using serial communication with the main processor of the board) but I'm always getting the error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;02: Failed on connect: Ee(02). Not connected to emulator.&lt;BR /&gt;Emu(0): Connected. Was: None. DpID: EDB6. Info=T1S6RGRIA&lt;BR /&gt;Err 0: (null)&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've tried the solutions from &lt;/SPAN&gt;&lt;A href="http://"&gt;http://lpcxpresso.code-red-tech.com/LPCXpresso/node/44&lt;/A&gt;&lt;SPAN&gt; . But the&amp;nbsp; ISP mode doesn't solve the problem neither the Vector catch does. I'm sure I'm getting into the ISP mode because the serial port of the processor stops replying as I programmed it, so the LPC1114 is not working anymore until I restart the board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And some extra info: Windows 7 32 bits Spanish. Software version 3.3.4 (version 3.4 doesn't even work for me on the sample LPC1114/301)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you have any idea or suggestion about why this can be happening I'll be really grateful.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Victor Pau&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:00:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Ee-02-on-custom-board-after-programming-sample-UART-code/m-p/545992#M9470</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:00:16Z</dc:date>
    </item>
    <item>
      <title>Re: Ee(02) on custom board after programming sample UART code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Ee-02-on-custom-board-after-programming-sample-UART-code/m-p/545993#M9471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Mon Jul 12 01:28:44 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This message is reporting that the debugger is unable to connect to the target. The most obvious reasons for this are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- you have run code on the target that has disabled the debug access or incorrectly set he clock (PLL)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- the target is crashing very early in the startup code&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(these problems should be resolved by the solutions you said you had tried)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- the SWD pins are not correctly connected.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you say the standard solutions don't work (and we have never known them to fail on correctly designed hardware) I would suggest that you review your SWD circuit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, you mentioned v3.4 doesn't work for you. What errors were reported?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:00:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Ee-02-on-custom-board-after-programming-sample-UART-code/m-p/545993#M9471</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:00:17Z</dc:date>
    </item>
    <item>
      <title>Re: Ee(02) on custom board after programming sample UART code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Ee-02-on-custom-board-after-programming-sample-UART-code/m-p/545994#M9472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by victorpau on Tue Jul 20 05:48:09 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I found the problem. It seems that while I was programming the chip I activated accidentally the CRP3, so the LPC1114 is completely isolated now. I've been using other micro-controllers before and I was expecting that the protection only avoided other people to read the code, not myself to program it again (As it's called Code Read Protection I didn't expect it to avoid writing)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So I think the only way that I have is to change the chip from the board for a new one, isn't it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It would be nice if LPCXpresso showed some warning when you choose to program the device with CRP3 so people doesn't do it by mistake.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Victor Pau&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:00:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Ee-02-on-custom-board-after-programming-sample-UART-code/m-p/545994#M9472</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:00:18Z</dc:date>
    </item>
    <item>
      <title>Re: Ee(02) on custom board after programming sample UART code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Ee-02-on-custom-board-after-programming-sample-UART-code/m-p/545995#M9473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by micrio on Tue Jul 20 07:34:58 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;If you have not provided a backdoor that erases the security word then you are dead.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you wnat to protect yourself in the future, you should implement a backdoor erase function. You could examine certain input pins and look for a special pattern and then erase all flash. You want to erase all flash, not just the security fuse. This should maintain security for your code.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If someone inadvertantly hits your secret I/O pin pattern then the device becomes useless to him so make sure that it will not happen in normal use.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:00:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Ee-02-on-custom-board-after-programming-sample-UART-code/m-p/545995#M9473</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:00:18Z</dc:date>
    </item>
  </channel>
</rss>