<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックLPC1768 deep-sleep Watchdog</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-deep-sleep-Watchdog/m-p/545796#M9382</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Goetz.Friedrich on Mon Mar 17 04:21:34 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi LPC experts,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;when selecting via WDCLKSEL the RTC as clock source for the WDT the LPC gets resetted in normal and in deep-sleep power mode as expected after WD timout.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When using IRC as WDT clock source only in normal power mode the reset occures as expected. In deep-sleep there is no reset seen (Using the same WTC configuration as in normal power mode)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the datasheet is mentioned:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;“The Watchdog timer can be configured to run in Deep Sleep mode when using the IRC as the clock source.”&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there something special which needs to be concidered using the IRC als clock source?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-Best regards, Götz-&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:35:06 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:35:06Z</dc:date>
    <item>
      <title>LPC1768 deep-sleep Watchdog</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-deep-sleep-Watchdog/m-p/545796#M9382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Goetz.Friedrich on Mon Mar 17 04:21:34 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi LPC experts,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;when selecting via WDCLKSEL the RTC as clock source for the WDT the LPC gets resetted in normal and in deep-sleep power mode as expected after WD timout.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When using IRC as WDT clock source only in normal power mode the reset occures as expected. In deep-sleep there is no reset seen (Using the same WTC configuration as in normal power mode)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the datasheet is mentioned:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;“The Watchdog timer can be configured to run in Deep Sleep mode when using the IRC as the clock source.”&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there something special which needs to be concidered using the IRC als clock source?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-Best regards, Götz-&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:35:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC1768-deep-sleep-Watchdog/m-p/545796#M9382</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:35:06Z</dc:date>
    </item>
  </channel>
</rss>