<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDEのトピックRe: Where are the LPC2xxx examples ?</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Where-are-the-LPC2xxx-examples/m-p/544899#M8949</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use the project wizard on the Quickstart Panel to create a new project for the part you are using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then extract the required example code from the appropriate code bundle for your part family.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc213xlpc214x-peripherals-using-keils-μvision" title="https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc213xlpc214x-peripherals-using-keils-μvision"&gt;Sample Code Bundle for LPC213x/LPC214x Peripherals using Keil's μVision | www.LPCware.com&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc23xxlpc24xx-peripherals-using-keils-μvision" title="https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc23xxlpc24xx-peripherals-using-keils-μvision"&gt;Sample Code Bundle for LPC23xx/LPC24xx Peripherals using Keil's μVision | www.LPCware.com&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should also take note of the debug probe requirements for ARM7&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389162"&gt;Which debug probes are supported by LPCXpresso IDE with which MCUs?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;[You basically need an LPC-Link (the original version, not the newer LPC-Link2) or a Red Probe+)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS : I would strongly recommend that you look at Cortex-M based MCUs - for instance the LPC1700 family for new product designs, rather than the older ARM7 based MCUs. This will provide you with much better software support and debgging capabilities.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jul 2016 08:13:42 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2016-07-27T08:13:42Z</dc:date>
    <item>
      <title>Where are the LPC2xxx examples ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Where-are-the-LPC2xxx-examples/m-p/544898#M8948</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently installed the LPCXpresso and I wasn't able to locate the LPC2xxx project examples. Can someone to provide more details about that ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 07:00:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Where-are-the-LPC2xxx-examples/m-p/544898#M8948</guid>
      <dc:creator>catalin_olteanu</dc:creator>
      <dc:date>2016-07-27T07:00:33Z</dc:date>
    </item>
    <item>
      <title>Re: Where are the LPC2xxx examples ?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Where-are-the-LPC2xxx-examples/m-p/544899#M8949</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can use the project wizard on the Quickstart Panel to create a new project for the part you are using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then extract the required example code from the appropriate code bundle for your part family.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc213xlpc214x-peripherals-using-keils-μvision" title="https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc213xlpc214x-peripherals-using-keils-μvision"&gt;Sample Code Bundle for LPC213x/LPC214x Peripherals using Keil's μVision | www.LPCware.com&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc23xxlpc24xx-peripherals-using-keils-μvision" title="https://www.lpcware.com/content/nxpfile/sample-code-bundle-lpc23xxlpc24xx-peripherals-using-keils-μvision"&gt;Sample Code Bundle for LPC23xx/LPC24xx Peripherals using Keil's μVision | www.LPCware.com&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should also take note of the debug probe requirements for ARM7&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389162"&gt;Which debug probes are supported by LPCXpresso IDE with which MCUs?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;[You basically need an LPC-Link (the original version, not the newer LPC-Link2) or a Red Probe+)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS : I would strongly recommend that you look at Cortex-M based MCUs - for instance the LPC1700 family for new product designs, rather than the older ARM7 based MCUs. This will provide you with much better software support and debgging capabilities.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 08:13:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Where-are-the-LPC2xxx-examples/m-p/544899#M8949</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-07-27T08:13:42Z</dc:date>
    </item>
  </channel>
</rss>