<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How Can I Clean Up Multiple LPXXpresso Setups? in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544729#M8832</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 27 00:58:00 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This is an artifact of Windows device drivers. They remain around because XP does not provide a convenient way of removing them (unlike Win7 etc, which does provide a convenient way of removing device drivers).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As you are using XP, I think you will either have to use a 3rd party tool to remove them, or you can try hand editing the registry (not recommended). Sorry,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Edit: BTW, they are benign. They are just occupying a bit of disk space.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:33:18 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:33:18Z</dc:date>
    <item>
      <title>How Can I Clean Up Multiple LPXXpresso Setups?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544728#M8831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Fri Sep 27 00:43:46 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am on XP Pro SP3.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have (currently) 5 or 6 installation of various flavours of the LPCXpresso IDE,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;including Code Red v3, v5, and RedSuite; NXP v6. I have previously installed and&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;deleted (some) up to 15 various versions -- V4/V5/RedSuite/V6&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It is claimed that the IDE setup does not use the registry (so I should be able to&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;simply delete the unwanted directories and desktop shortcuts).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;BUT, what about the 'Start Menu' and registry 'Uninstall' Items? (I haven't looked yet).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ALSO 'Documents and Setings (all users)' has LPCXpresso, RedSuite5, and NXPLPCXpresso&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;folders (for the licences?). I'm guessing that I can delete a;; but NXPLPCXpresso?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;A much bigger issue is the state of LPC-Link and LPC-Link2 driver stuff.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Even though I obly have ONE LPC-Link and ONE LPC-Link2 device, there are apparently&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;multiple device entries. [Text and html lists attached.]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you provide a tool to COMPLETELY remove all LPC-Link 1/2 from the system and the registry.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And then explain how to reinstall JUST the latest (IDE V6) driver WITHOUT having to reinstall&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the V6 setup program.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards, Mike.&lt;/SPAN&gt;&lt;BR /&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338191"&gt;LPC-Link-List.html_.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338191"&gt;LPC-Link-List.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544728#M8831</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:33:17Z</dc:date>
    </item>
    <item>
      <title>Re: How Can I Clean Up Multiple LPXXpresso Setups?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544729#M8832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 27 00:58:00 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;This is an artifact of Windows device drivers. They remain around because XP does not provide a convenient way of removing them (unlike Win7 etc, which does provide a convenient way of removing device drivers).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As you are using XP, I think you will either have to use a 3rd party tool to remove them, or you can try hand editing the registry (not recommended). Sorry,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Edit: BTW, they are benign. They are just occupying a bit of disk space.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544729#M8832</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:33:18Z</dc:date>
    </item>
    <item>
      <title>Re: How Can I Clean Up Multiple LPXXpresso Setups?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544730#M8833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 27 01:05:43 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;After a bit of searching, I found this trick to show 'Hidden' devices in Device Manager&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.techrepublic.com%2Farticle%2Fremoving-unused-device-drivers-from-windows-xp-machines%2F" rel="nofollow" target="_blank"&gt;http://www.techrepublic.com/article/removing-unused-device-drivers-from-windows-xp-machines/&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This provides a way to list 'unused' devices and to uninstall them.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hope that helps&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544730#M8833</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:33:18Z</dc:date>
    </item>
    <item>
      <title>Re: How Can I Clean Up Multiple LPXXpresso Setups?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544731#M8834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Fri Sep 27 01:13:09 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the hint.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I found these entried using UsbDViewf from nirsoft.net&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you comment about the license files in Docs+Settings?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers, Mike&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544731#M8834</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:33:19Z</dc:date>
    </item>
    <item>
      <title>Re: How Can I Clean Up Multiple LPXXpresso Setups?</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544732#M8835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 27 01:26:13 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;On Windows XP, the license files are stored in &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;%ALLUSERSPROFILE%&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;which is an environment variable whose value is typically "C:\Documents and Settings\All Users"`&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The license files are stored in sub-directories:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Red Suite 5.x: RedSuite5&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Red Suite 4.x: RedSuite&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]Red Suite 3.x: red_suite&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]LPCXpresso: LPCXpresso &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If you are not using the product, just delete the directory.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:33:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/How-Can-I-Clean-Up-Multiple-LPXXpresso-Setups/m-p/544732#M8835</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:33:19Z</dc:date>
    </item>
  </channel>
</rss>