<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Linker error in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-error/m-p/544523#M8741</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Thu Aug 05 06:06:35 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;A few suggestions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- have you set up the Library paths in the linker, so that it can find the Library? It will need to reference ${workspace_loc:[SIZE=2]CMSISv1p30_LPC11xx/Debug} or [/SIZE]${workspace_loc:[SIZE=2]CMSISv1p30_LPC11xx/Release} depending own whather you want a debug or release build&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Is the library actually built in that location? It will be looking for a file called lib[/SIZE][SIZE=2]CMSISv1p30_LPC11xx.a[/SIZE]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 22:04:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T22:04:01Z</dc:date>
    <item>
      <title>Linker error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-error/m-p/544522#M8740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Kees Jansen on Thu Aug 05 05:48:23 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Dear alll,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I made a new workbench with LPXxpresso according the "Getting Started" document. The workbench consist of the CMSISv1p30_LPC11xx project and a new own project. My own project uses the CMSISv1p30_LPC11xx . I received the following message after compiling/making&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[SIZE=2][LEFT]c:/nxp/lpcxpresso_3.4/tools/bin/../lib/gcc/arm-none-eabi/4.3.3/../../../../arm-none-eabi/bin/ld.exe: cannot find -lCMSISv1p30_LPC11xx&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;collect2: ld returned 1 exit status[/LEFT]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make: *** [LPC11xxMicroCoreI2cBlinky.c.axf] Error 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I compared the workbench with a similar workbench that can be compiled and made. I did not find differences in the properties of the projects (other than names)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anybody know what I have to do to get rid of the error. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What kind of file does the ld.exe want? Where can I tell him that in LPCxpresso?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Hoping somebody can help me,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Kees. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/SIZE]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-error/m-p/544522#M8740</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:04:00Z</dc:date>
    </item>
    <item>
      <title>Re: Linker error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-error/m-p/544523#M8741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Thu Aug 05 06:06:35 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;A few suggestions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- have you set up the Library paths in the linker, so that it can find the Library? It will need to reference ${workspace_loc:[SIZE=2]CMSISv1p30_LPC11xx/Debug} or [/SIZE]${workspace_loc:[SIZE=2]CMSISv1p30_LPC11xx/Release} depending own whather you want a debug or release build&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Is the library actually built in that location? It will be looking for a file called lib[/SIZE][SIZE=2]CMSISv1p30_LPC11xx.a[/SIZE]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-error/m-p/544523#M8741</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:04:01Z</dc:date>
    </item>
    <item>
      <title>Re: Linker error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-error/m-p/544524#M8742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Kees Jansen on Thu Aug 05 07:17:57 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for the (fast)&amp;nbsp; reply. Indeed the path to the library was wrong. :)Was great help to know that *.a is the library extension. My mistake was the interpretation of the "workbench" button. You have to define the whole path in the workbench directory too Not pointing to the workbench directory itself.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The debugger however is not working .:( I see some mistakes in the command lines &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MicroCoreI2CBlinky files are MicroCoreI2CBlinky.c.axf and MicroCoreI2CBlinky.c.map . That's wrong to my opinion. It should be &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MicroCoreI2CBlinky.axf&amp;nbsp; and MicroCoreI2CBlinky.map.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there a possiblilty to correct that in LPCXpresso?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Hoping you can help,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Kees&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-error/m-p/544524#M8742</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:04:02Z</dc:date>
    </item>
    <item>
      <title>Re: Linker error</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-error/m-p/544525#M8743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Thu Aug 05 09:15:36 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;That will because your project name is "MicroCoreI2CBlinky.c" (or at leaast, that was the name of the project when your created it). If you want to change the name of your "build artifact", &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Project-&amp;gt;Properties,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;C/C++ Build&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Settings&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Click the "Build artifact" tab&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;change the Build artifact name to whatever you want. That will affect the .axf and the .map (and anything else that uses the BuildArtifactBaseName).&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 22:04:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Linker-error/m-p/544525#M8743</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T22:04:02Z</dc:date>
    </item>
  </channel>
</rss>