<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC11C24 Problems with the CAN Tx Callback in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C24-Problems-with-the-CAN-Tx-Callback/m-p/544453#M8710</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Abandoner on Wed Aug 08 14:07:07 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the LPC11C24 with the Xpresso Board and also in custom designs. My problem is sending CAN Messages at a "short" period like 10 to 50 ms. It is causing a halt (All my CAN_TX Buffers are busy) after about 100 to 200 Messages and the CAN_Tx Callback&amp;nbsp; is not called anymore.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[EDIT] Solved : I used an bitwise "&amp;amp;" instead of "&amp;amp;&amp;amp;" in an if statement&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:50:18 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:50:18Z</dc:date>
    <item>
      <title>LPC11C24 Problems with the CAN Tx Callback</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C24-Problems-with-the-CAN-Tx-Callback/m-p/544453#M8710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Abandoner on Wed Aug 08 14:07:07 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the LPC11C24 with the Xpresso Board and also in custom designs. My problem is sending CAN Messages at a "short" period like 10 to 50 ms. It is causing a halt (All my CAN_TX Buffers are busy) after about 100 to 200 Messages and the CAN_Tx Callback&amp;nbsp; is not called anymore.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[EDIT] Solved : I used an bitwise "&amp;amp;" instead of "&amp;amp;&amp;amp;" in an if statement&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C24-Problems-with-the-CAN-Tx-Callback/m-p/544453#M8710</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11C24 Problems with the CAN Tx Callback</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C24-Problems-with-the-CAN-Tx-Callback/m-p/544454#M8711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Ex-Zero on Wed Aug 08 14:26:29 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Abandoner&lt;/STRONG&gt;&lt;BR /&gt;Does anyone have any suggestions?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Reduce you project as far as you can and post it. That's easier than answering thousand questions :eek:&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:50:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPC11C24-Problems-with-the-CAN-Tx-Callback/m-p/544454#M8711</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:50:19Z</dc:date>
    </item>
  </channel>
</rss>