<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Lpcxpresso debug session in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Lpcxpresso-debug-session/m-p/528201#M836</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bhallett on Tue Sep 21 02:20:04 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have LPCXpresso v 3.3.4 installed on my PC which I have not used for approx 10 months. Now that I want to use it again I am having trouble using the debug mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem im having has the following symptom:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- I set the IDE to start up in debug mode,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- I set a break point,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- Start my debug session&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- Session stops on break point&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- I try to use 'Step Into' F5 or 'Step Over' F6&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then the IDE does not do what it used to do and that is to step to the next line, instead, a new window opens up labled 1 "&amp;lt;symbol is not available&amp;gt; 0" containing Red text "No source available for """ and a button labled "View Disassembly".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If i press F5 or F6 again an error message reporting "Execution is suspended because of error" is reported.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone help ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Barry&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:05:16 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:05:16Z</dc:date>
    <item>
      <title>Lpcxpresso debug session</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Lpcxpresso-debug-session/m-p/528201#M836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bhallett on Tue Sep 21 02:20:04 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have LPCXpresso v 3.3.4 installed on my PC which I have not used for approx 10 months. Now that I want to use it again I am having trouble using the debug mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem im having has the following symptom:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- I set the IDE to start up in debug mode,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- I set a break point,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- Start my debug session&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- Session stops on break point&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- I try to use 'Step Into' F5 or 'Step Over' F6&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then the IDE does not do what it used to do and that is to step to the next line, instead, a new window opens up labled 1 "&amp;lt;symbol is not available&amp;gt; 0" containing Red text "No source available for """ and a button labled "View Disassembly".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If i press F5 or F6 again an error message reporting "Execution is suspended because of error" is reported.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone help ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Barry&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:05:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Lpcxpresso-debug-session/m-p/528201#M836</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:05:16Z</dc:date>
    </item>
    <item>
      <title>Re: Lpcxpresso debug session</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Lpcxpresso-debug-session/m-p/528202#M837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CodeRedSupport on Tue Sep 21 02:42:48 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Not sure how you have managed to be using 3.3.4 for 10 months - it was only released in mid-April :D Note that the current release version of LPCXpresso is 3.5.0 - you can install this in parallel to your existing 3.3.4 installation by selecting a different installation directory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Anyway, with regards to your problem, are you seeing this with a project that you created sometime ago? Did you rebuild it before debugging?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I would certainly suggest doing a clean and build and trying to debug again.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; Can you check that the build options are specifying that debug is&amp;nbsp; turned on for all your files - in particular the one containing the code&amp;nbsp; which causes the display of the error when you step into it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you also confirm if you can successfully debug any of the supplied examples for your target MCU, or is the issue specific to this one project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It is also possible that something might have corrupted your workspace. It might be worth exporting your project to a zip file via the Quickstart Panel, then importing it back into a completely new workspace project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If this still doesn't work, please can you do a clean and build, then copy'n'paste the build log into a text file and post here.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;CodeRedSupport&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:05:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Lpcxpresso-debug-session/m-p/528202#M837</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:05:17Z</dc:date>
    </item>
    <item>
      <title>Re: Lpcxpresso debug session</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Lpcxpresso-debug-session/m-p/528203#M838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bhallett on Tue Sep 21 02:48:58 MST 2010&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello CodeRedSupport,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Apologies to all, I have managed to resolve my issue. When building the code for final release I specifically enable the watchdog timer as a result affects the debug facility. In order to use the debug facility I disable enabling the watchdog.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Barry&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:05:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Lpcxpresso-debug-session/m-p/528203#M838</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:05:18Z</dc:date>
    </item>
  </channel>
</rss>