<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 Re: LPCExpresso install on USB thumb drive</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCExpresso-install-on-USB-thumb-drive/m-p/528199#M834</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Wed Dec 10 02:11:59 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;When it was Code Red, they said that it did not use any registry.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, the licence file(s?) goes in "Documents and Settings"/"User" &amp;lt;yourname&amp;gt;/something&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And debugging etc. runs scripts that need a windows "cscript?" somewhere on the path.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also USB device drivers are installed (on the PC) at installation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So probably not.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, Java bloatware is huge so you would need a big memory stick.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My 7.4 installation on Win7-64 is 741 megabytes. That's without the workspaces.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 00:15:43 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T00:15:43Z</dc:date>
    <item>
      <title>LPCExpresso install on USB thumb drive</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCExpresso-install-on-USB-thumb-drive/m-p/528197#M832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rocketdawg on Tue Dec 09 17:00:57 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am wondering whether or not LPCExpresso and LPCOpen and workspaces can all be installed on a thumb driver.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the goal is to have a complete portable development environment.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So the real question is how much junk does Eclipse and other packages place in the registry?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:15:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCExpresso-install-on-USB-thumb-drive/m-p/528197#M832</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:15:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPCExpresso install on USB thumb drive</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCExpresso-install-on-USB-thumb-drive/m-p/528198#M833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Wed Dec 10 02:09:50 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso does not use the Registry directly (although the installer does place some install/uninstall information there, it is not used by the product when running).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We have not tried it, but I don't see any reason why it should not work, subject to the following caveats:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- If you want to debug, drivers for USB debug adapters will need to be installed on each machine. They can be found in the Drivers directory of the install directory&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Any target machine will need the Visual Studio redistributables installed. Many machines have these installed, but if not, you need to run the vcredist_x86.exe installer found in the install directory&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Performance is likely to be slow. The IDE uses its install directory to cache a lot of (run time) information. USB flash drives are typically very slow for this sort of information&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- There is some configuration information stored in the "configuration" (!) directory. Some of this includes path information, including the drive letter. I don't expect this to cause any significant problems&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- Workspaces are not designed to be portable like this. They will contain full paths that are likely to cause issues when moving between machines of the USB flash drive has a different drive letter (i.e E: or F:). However, you can normally recover this by using File-&amp;gt;Import, General/Existing projects into workspace&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There may be others, but these are the ones that I can think of immediately. All I can suggest is - try it and report back your findings. Good luck.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:15:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCExpresso-install-on-USB-thumb-drive/m-p/528198#M833</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:15:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPCExpresso install on USB thumb drive</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCExpresso-install-on-USB-thumb-drive/m-p/528199#M834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Wed Dec 10 02:11:59 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;When it was Code Red, they said that it did not use any registry.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, the licence file(s?) goes in "Documents and Settings"/"User" &amp;lt;yourname&amp;gt;/something&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And debugging etc. runs scripts that need a windows "cscript?" somewhere on the path.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also USB device drivers are installed (on the PC) at installation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So probably not.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, Java bloatware is huge so you would need a big memory stick.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My 7.4 installation on Win7-64 is 741 megabytes. That's without the workspaces.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mike &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCExpresso-install-on-USB-thumb-drive/m-p/528199#M834</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:15:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPCExpresso install on USB thumb drive</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/LPCExpresso-install-on-USB-thumb-drive/m-p/528200#M835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rocketdawg on Wed Dec 10 16:50:08 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks, I'll try it and see.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;slow does not matter as much as the convenience of take-it-anywhere.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And I really just want to write and compile code.&amp;nbsp; I can debug on my main dev PC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can sync up source code from a solution folder to my main development PC when I make changes. &lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 00:15:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/LPCExpresso-install-on-USB-thumb-drive/m-p/528200#M835</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T00:15:44Z</dc:date>
    </item>
  </channel>
</rss>