<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question on driving stepper motors in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Question-on-driving-stepper-motors/m-p/543536#M8293</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Dave3891 on Wed Jul 13 23:01:39 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on a 6 axis stepper signal generator (Step and Direction) and I have tried a few different ways but I can't seem to get the max freq that I am looking to be close to (1Mhz).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the LPC1343&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am just looking for advice on the fastest way to do it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My current idea is to use the 2 32bit timers with 3 match registers on each timer, but I would have to use a free running timer and do a matchReg++ on each interrupt and a position++ for each interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When the match is in toggle mode, how long does it toggle for?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have also tried a version that uses Bresenham formula and one timer, but this one could not interpolate all 6 axis faster then about 200khz...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So I am looking to have all 6 axis running at a max of 1MHz and I am not sure of the best way to do this and if it would work with the 2 timers and 6 match registers...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Dave&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:51:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:51:57Z</dc:date>
    <item>
      <title>Question on driving stepper motors</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Question-on-driving-stepper-motors/m-p/543536#M8293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Dave3891 on Wed Jul 13 23:01:39 MST 2011&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on a 6 axis stepper signal generator (Step and Direction) and I have tried a few different ways but I can't seem to get the max freq that I am looking to be close to (1Mhz).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using the LPC1343&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am just looking for advice on the fastest way to do it.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My current idea is to use the 2 32bit timers with 3 match registers on each timer, but I would have to use a free running timer and do a matchReg++ on each interrupt and a position++ for each interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When the match is in toggle mode, how long does it toggle for?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have also tried a version that uses Bresenham formula and one timer, but this one could not interpolate all 6 axis faster then about 200khz...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So I am looking to have all 6 axis running at a max of 1MHz and I am not sure of the best way to do this and if it would work with the 2 timers and 6 match registers...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Dave&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:51:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Question-on-driving-stepper-motors/m-p/543536#M8293</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:51:57Z</dc:date>
    </item>
  </channel>
</rss>