<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPCXpresso IDE中的主题 UART problem with the relocated application code</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-problem-with-the-relocated-application-code/m-p/528172#M819</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Dore on Wed Dec 18 03:56:23 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have written a small app code in which UART, Timer are there along with one external GPIO interrupt. A boot code which is for application upgrade through my specific commands.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have moved my app code to 0x1000 and my boot code starts at 0x000.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In this case with my boot code the UART communication works, I am able to send and receive commands responses w.r.t my own protocol format.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the same in app code. Both individually works fine. But when I relocate the application to 0x1000 onwards the app code's UART communication doesnt respond most of the times, rarely it responds for my commands.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there something specifically I should take care at this scenario.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 02:53:07 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T02:53:07Z</dc:date>
    <item>
      <title>UART problem with the relocated application code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-problem-with-the-relocated-application-code/m-p/528172#M819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Dore on Wed Dec 18 03:56:23 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have written a small app code in which UART, Timer are there along with one external GPIO interrupt. A boot code which is for application upgrade through my specific commands.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have moved my app code to 0x1000 and my boot code starts at 0x000.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In this case with my boot code the UART communication works, I am able to send and receive commands responses w.r.t my own protocol format.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the same in app code. Both individually works fine. But when I relocate the application to 0x1000 onwards the app code's UART communication doesnt respond most of the times, rarely it responds for my commands.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Is there something specifically I should take care at this scenario.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:53:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-problem-with-the-relocated-application-code/m-p/528172#M819</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:53:07Z</dc:date>
    </item>
    <item>
      <title>Re: UART problem with the relocated application code</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/UART-problem-with-the-relocated-application-code/m-p/528173#M820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by MikeSimmonds on Wed Dec 18 10:22:24 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Sounds like a vector table relocation (i.e. you have not) issue.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Cheers, Mike&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 02:53:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/UART-problem-with-the-relocated-application-code/m-p/528173#M820</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T02:53:08Z</dc:date>
    </item>
  </channel>
</rss>