<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem with switching between power-down-mode and sleep-mode (LPC1769) in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-switching-between-power-down-mode-and-sleep-mode/m-p/542844#M7993</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CroesJeroen on Fri Aug 10 14:36:49 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I thought you could only use one of the modes. Like sleep, deep sleep or deep power down. I think you can't use two at the same time, that's why 3 modes are defined ( I think so)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 01:51:03 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-16T01:51:03Z</dc:date>
    <item>
      <title>Problem with switching between power-down-mode and sleep-mode (LPC1769)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-switching-between-power-down-mode-and-sleep-mode/m-p/542843#M7992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ledmaster on Fri Aug 10 02:44:19 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello, in my application I'm switching between the two energy-safe-modes power-down and sleep.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I can only use sleep or&amp;nbsp; power-down, but if I want to use both of them, the switch from power-down to sleep will cause the controller to reset while writing "0x00" to PCON.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anybody have this problem too?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Yannick&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-switching-between-power-down-mode-and-sleep-mode/m-p/542843#M7992</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:51:02Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with switching between power-down-mode and sleep-mode (LPC1769)</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-switching-between-power-down-mode-and-sleep-mode/m-p/542844#M7993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by CroesJeroen on Fri Aug 10 14:36:49 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I thought you could only use one of the modes. Like sleep, deep sleep or deep power down. I think you can't use two at the same time, that's why 3 modes are defined ( I think so)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 01:51:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Problem-with-switching-between-power-down-mode-and-sleep-mode/m-p/542844#M7993</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-16T01:51:03Z</dc:date>
    </item>
  </channel>
</rss>