<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Download/Debug Limit Clarification in LPCXpresso IDE</title>
    <link>https://community.nxp.com/t5/LPCXpresso-IDE/Download-Debug-Limit-Clarification/m-p/542648#M7918</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by martinmckee on Fri Feb 28 18:54:52 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm looking to use an LPC4330 in an upcoming application.&amp;nbsp; In most ways, it is the perfect device for the application which requires both low latency ( which could be handled by the dual core structure and high clock speed ) and it is also computation limited.&amp;nbsp; What it does not need is a large amount of program memory -- the application will easily fit under the 256k limit.&amp;nbsp; I just wanted to check that a SPIFI connected memory could be programmed if the actual code remains under the 256k.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Martin Jay McKee&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 23:21:30 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T23:21:30Z</dc:date>
    <item>
      <title>Download/Debug Limit Clarification</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Download-Debug-Limit-Clarification/m-p/542648#M7918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by martinmckee on Fri Feb 28 18:54:52 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm looking to use an LPC4330 in an upcoming application.&amp;nbsp; In most ways, it is the perfect device for the application which requires both low latency ( which could be handled by the dual core structure and high clock speed ) and it is also computation limited.&amp;nbsp; What it does not need is a large amount of program memory -- the application will easily fit under the 256k limit.&amp;nbsp; I just wanted to check that a SPIFI connected memory could be programmed if the actual code remains under the 256k.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Martin Jay McKee&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:21:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Download-Debug-Limit-Clarification/m-p/542648#M7918</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:21:30Z</dc:date>
    </item>
    <item>
      <title>Re: Download/Debug Limit Clarification</title>
      <link>https://community.nxp.com/t5/LPCXpresso-IDE/Download-Debug-Limit-Clarification/m-p/542649#M7919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Sat Mar 01 04:38:53 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Yes - downloads to such as system is fine as long as the code size is &amp;lt; 256KB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso Support&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 23:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPCXpresso-IDE/Download-Debug-Limit-Clarification/m-p/542649#M7919</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T23:21:31Z</dc:date>
    </item>
  </channel>
</rss>